STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

noisy audio recording after averaging data

I am using F446 board with CCA02m2.when I just send the audio to USB output, I can record data in audacity. But if I do simple processing such as averaging data, the output is high clipped data.I checked the data range and overflowing. there is no pr...

FTEHR.1 by Associate
  • 1229 Views
  • 1 replies
  • 0 kudos

Get data from USB_ReadPacket function

I am using a STM32F4 on a custom board with USB configured as custom hid device.I need to know how to get the received data from the USB_ReadPacket placed inside the HAL_PCD_IRQHandler (I suppose this is the function called when the device receive da...

VCapu by Associate III
  • 1895 Views
  • 4 replies
  • 0 kudos

How can drive this USB_HRF1036 via Python?

Hello All,I bought a USB to DAQ board from a very lousy company DAQVANTech.Due to very poor support, I would like to try ST forum.The board is like the attachments.And, it uses STM32F103VCT6 as you can see on the screenshot.I very appreciate if anyon...

Resolved! Can't Ping Device After Writing to QSPI w/ RTOS

I have full IwIP functionality inside a RTOS task due to this knowledge article: How to create project for STM32H7 with Ethernet and LwIP stack workingI am able to erase, write, and read the QSPI flash using a BSP_QSPI test function inside main. Thi...

DWill.4 by Associate II
  • 5817 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L422 High current consumption in STOP 2 mode

Hello, We are trying to put an STM32L422 MCU to STOP 2 mode but the pcb consumption is high (~60uA). The PCB is not to blame because when the MCU enters STANDBY mode, the current consumption is ~5uA. In order to set up the MCU to enter STOP 2 mode, w...

ZPapa.1 by Associate II
  • 2460 Views
  • 2 replies
  • 0 kudos

azure RTOS connectivity with Nucleo-h745zi-q?

I am working on a Nucleo-h745zi-q controller. I want to connect the stm32h7 board with Microsoft azure. I installed the package on stm32ide x-cube-azrtos-h7. But I did not know how I can connect to azure. What is the procedure for using this Rtos con...

Kk1 by Associate II
  • 3166 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H7x USB Dual Role

Hi,I am currently working on a project that needs the support of the USB dual role functionality of STM32H75x controller. Is there any example that I can use as a base, or if there are any guidelines please direct them to me. More details,Individual ...

CDiss.1 by Associate
  • 1622 Views
  • 1 replies
  • 0 kudos

Problem with getting time and date

Hello everyone,I'm using STM32L496G-Discovery_Azure example of x_cube_azure package on my custom board and I have some problems when trying to connect to network to get network time for internal RTC. First steps of the function setRTCTimeDateFromNetw...

NCatt.1 by Associate III
  • 995 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.