STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Printer with STM32

How would I go about implementing a USB host for a usb printer. I would like to send things through my STM32 to be printed. I’ve seen adaptations or some work done on the USB printer class as a device but I am unsure how I would do this as a host? An...

Resolved! STM32Cubeide 2.0

Hi there!i start one of my new project with STM32cubeide 2.0. First i start with configure mu MCU in STM32CUBEMX in this casa STM32G031K8T6 afther i configurate all pin i create a poject . So afther i import my project in STM32CubeIde 2.0 and i build...

SGian.1 by Senior
  • 540 Views
  • 4 replies
  • 0 kudos

Resolved! Bugs in sd_diskio.c alignment handling

I've had problems with sd_diskio.c used for SD card I/O with FatFs.CubeMX version is 6.16.0.I'm using SDMMC with DMA, so consideration needs to be given to cache coherency and alignment.I have both these set:#define ENABLE_SD_DMA_CACHE_MAINTENANCE  1...

USB device not recognized with RNDIS using USBX

Hello,I am trying to get Ethernet-over-USB working on a STM32U585. I want to be able to use both RNDIS and CDC-ECM, but I decided to start with RNDIS first. After a lot of trial and error and research, I am running out of ideas as to why my PC does n...

KoCT by Associate II
  • 545 Views
  • 1 replies
  • 0 kudos

Sending Status without sending VDO

我使用的芯片是G071RB,当我使用STM32UCPD发status,直接从FF01(PD协议的DP模式)变成0x00000,并且在抓包发现再发送的时候没有发VDO000000001,返回的数据中HPD为0,有没有大佬知道怎么解决 Translation: I'm using the STM32G071RB MCU. When I send a status update using STM32UCPD, it jumps directly from FF01 (DP mode of the P...

Shirly_X by Associate
  • 310 Views
  • 1 replies
  • 0 kudos

Resolved! The STM32H743 LPuart+DMA_IDLE does not function properly

下面是我的部分函数,普通串口按照这个配置,是可以正常进入回调函数,但是LPuart却不能进入回调函数,不知道问题出在哪里,使用stm32cubemx6.16.0,附件是ioc文件,   Post Edited by ST moderator to apply source code formatting and translate from Chinese to English to comply with the community rule:   Below are some of my ...

ymy by Associate II
  • 641 Views
  • 6 replies
  • 3 kudos

USB CDC packet loss at high data rates

When using a USB CDC device, especially at high data rates, there is a possibility for packet loss. This post illustrates the issue with what I consider convincing evidence. This isn't a STM32 bug, but it's something you may encounter when interfacin...

TDK_1-1766165272664.png TDK_2-1766165357056.png TDK_0-1766165197615.png
TDK by Super User
  • 1943 Views
  • 8 replies
  • 9 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.