STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 MW USB Device Library v2.8.0 release on GitHub

What is new in STM32 USB Device Library v2.8.0? *         Integration of new USB device Class driver: USB Printer Class driver based on Universal Serial Bus Device Class Definition for Printing Devices Version 1.1 *         USB All Classes: Fix USB b...

Resolved! 1.8V VDD and 3.3V IO

I am utilizing the STM32F767ZI in a design and am wondering if the following will cause any issues. I have VDD set to 1.8V so the standard IO is 1.8V, however, JTAG and USB-DFU control use 3.3V standard.Based on the DS, the corresponding pins (PA11-1...

CPetr.2 by Associate
  • 2735 Views
  • 2 replies
  • 0 kudos

How to debug in udp_echoserver_receive_callback function when implementing udp echo server on Nucleo-F439zi

Hey, Have a question about how to debug in the udp_receive_callback function. In fact, I have done some stuff there but I am trying to debug there (put breakpoints inside of udp_receive_callback but it never goes there ...) without success until now....

0693W00000DqN0yQAF.png 0693W00000DqN0UQAV.png
LBadi.1 by Associate II
  • 1555 Views
  • 1 replies
  • 1 kudos

Hello I want select inbuilt USB Microcontroller with Support HID, Cost of Minimum Quantity, Product life cycle, Availability and lead time, Also alternative part number.

Hello I want select inbuilt USB Microcontroller with Support HID, Cost of Minimum Quantity, Product life cycle, Availability and lead time, Also alternative part number. So I hope you will be give me some response on this. One of the Part number has...

Svish.3 by Associate
  • 1108 Views
  • 1 replies
  • 0 kudos

stm32h723zg

Hi,I’m trying to use example from stmCubeIde (LwIP_TCP_Echo_Server LwIP TCP Echo Server Application) for NUCLEO144 with stm32h723zg, this application return the echo of the inserted character.I try to use putty (with ip and port) and it works, the pr...

GNobi.1 by Associate II
  • 1369 Views
  • 1 replies
  • 0 kudos

Resolved! Setting up USB HS FIFO size for STM32H745

Hi. I'm trying to migrate from USB FS to HS composite device on STM32H745. FS device (VCP+MSM) works fine, the settings for FIFO are: HAL_PCDEx_SetRxFiFo( &hpcd_USB_OTG_FS, 0x80 ); // RxFIFO:     HAL_PCDEx_SetTxFiFo( &hpcd_USB_OTG_FS, 0, 0x40 ); // E...

SLuka.1 by Associate II
  • 2755 Views
  • 2 replies
  • 0 kudos

My program goes into Hardfault_handler during enabling interrupt routing for SPI interfacing with TI Wi-Fi module[cc3135] using freeRTOS_POSIX.

My project is to publish/subscribe data between STM32H750 MCU and AWS cloud. For that I used to interface CC3135 Wi-Fi module for TI with my MCU. I am using freeRTOS_POSIX driver to communicate Wi-Fi module via SPI bus. I had successfully ported demo...

HPosh.1 by Associate
  • 1259 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.