2021-09-08 9:10 AM
I am utilizing the STM32F767ZI in a design and am wondering if the following will cause any issues. I have VDD set to 1.8V so the standard IO is 1.8V, however, JTAG and USB-DFU control use 3.3V standard.
Based on the DS, the corresponding pins (PA11-14, PB3, NRST) are all FT meaning they are 5V tolerant. So, am I correct in assuming that I can use the 3.3V JTAG/USB-DFU without needing level shifters to bring them down to 1.8V?
Solved! Go to Solution.
2021-09-08 9:29 AM
> ... USB-DFU control use 3.3V standard.
USB has its own differential signal control. Not really equivalent to a "3.3V standard".
USB requires VDDUSB of at least 2.7V, per the datasheet. If you have VDDUSB = VDD = 1.8V, it won't work.
Not sure on JTAG.
2021-09-08 9:29 AM
> ... USB-DFU control use 3.3V standard.
USB has its own differential signal control. Not really equivalent to a "3.3V standard".
USB requires VDDUSB of at least 2.7V, per the datasheet. If you have VDDUSB = VDD = 1.8V, it won't work.
Not sure on JTAG.
2021-09-08 11:56 AM
Ah you're right, I just tested the USB-DFU and it wasn't detected below 2.2V VDD so level shifters are the way to go. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.