STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

With BFB2 set on an STM32F429 (i.e. the ROM bootloader runs before the application code) it is not possible to start an application that runs from the flash alias at address 0. That works fine with BFB2=0.

STM32F429.The problem appears after the bootloader has run and jumped to application code, which it does when BFB2=1. When my application reads data from addresses around 0, it gets data from the ROM bootloader instead of from flash. I.e. it behaves ...

Wocket by Associate
  • 1601 Views
  • 2 replies
  • 1 kudos

Resolved! Azure FileX sd driver issue

Hello ST community,I believe there is an issue with the code generated by CubeMX for the fx_stm32_sd_driver. Config used :STM32CubeIDE : 1.10.1STM32U5 Cube Package : 1.1.1STM32CubeMX : 6.6.1In CubeMX, when I set the "FX Driver Initializes the SD IP" ...

0693W00000WHrw0QAD.png 0693W00000WHrwPQAT.png
CGuil.1 by Associate II
  • 1805 Views
  • 2 replies
  • 1 kudos

STM32G07 bootloader not starting

I had a hard time the last days struggling with STM32G07 bootloader.Finally I came to this conclusion:I have option bit nBOOT_SEL cleared (unckecked in STCubePorgrammer) and even though this bit is long cleared ie several power cycles have been done ...

How to add FreeRTOS to BLE Serial Port Example?

I refer to the BLE Beacon FreeRTOS example and include the FreeRTOS file into the BLE Serial Port example, but the RAM exceeds 1808 Byte, so I modified FreeRTOSConfig.h and adjusted the constants related to SIZE, but it still failed.I would like to a...

J.C by Associate
  • 1145 Views
  • 0 replies
  • 0 kudos

SPI_RxFIFOThresholdConfig is not defined

I'm using the L4xx HAL library and trying to set my SPI RX threshold value to 1/4 so I can receive a single byte response. From my research there should be a HAL function called SPI_RxFIFOThresholdConfig that will do this. When I put it into my SPI i...

RBair.3 by Associate II
  • 1801 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.