STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet TX doesn't work because ETH_DMATxDescListInit() doesn't initialize the entire ETH_DMADescTypeDef

The officially recommended recipe for lwIP on STM32H7 puts the ethernet DMA descriptors in SRAM1. SRAM1 is not zero'd by the default startup code.It's unsafe for the network drivers to assume that buffers and critical data structures live in .bss.F...

Resolved! I have a question about cmsis dsp lib source.((arm_mult_q31.c)

Hi​I found something strange in cmsis dsp source.​I am using stm32f429 and LITTLE ENDIAN and cmsis dsp library V.1.5.1.​in cmsis dsp library(arm_mult_q31.c) :​void arm_mult_q31( q31_t * pSrcA, q31_t * pSrcB, q31_t * pDst, uint32_t blockSize){... whil...

yh by Associate II
  • 4395 Views
  • 4 replies
  • 0 kudos

SPI is always stuck in busy state

I have found several other forum posts on this subject, and I've tried to follow them, but I'm still stuck. For some reason, SPI3 on my bl47eio1a never enters a ready state. It gets stuck waiting for a ready state before it ever can send or receive a...

RBair.3 by Associate II
  • 4176 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeMonitor-UCPD "message rejected for this port configuration" when requesting Power Profile

Hello, I'm able to connect the STM32CubeMonitor-UCPD with NUCLEO-G071RB and X-NUCLEO-SNK1M after following the instructions in AN5418. I only changed port 0 Sink PDO1 to 0x020641F4.I want to use the setup as a sink and always want to get the maximum ...

AlexH by Associate
  • 4325 Views
  • 3 replies
  • 0 kudos

STM32H7 SPI low level driver

I am trying to run the SPI peripheral on STM32H757 using low level drivers but no luck at all. The STM32cube H7 package contains example for controllers which has no FiFO, . Thus the examples cant be directly use. Also i have cherry picked quite alot...

JTari.1 by Associate II
  • 1937 Views
  • 1 replies
  • 0 kudos

STM32H743 Ethernert AIS Interrupt

Hey together,I have a question regarding the STM32H7 ethernet interrupts. I have lwIP + freeRTOS running successfully on the device. All fixes which were indicated by @alister​ were applied and it runs quite stable. The strange part is that when I ap...

0693W00000VOMlzQAH.png 0693W00000VOMmEQAX.png
ESawa.1 by Senior
  • 2981 Views
  • 4 replies
  • 0 kudos

Using USB HS with DMA in STM32F7

Hi,I am currently writing an application for a STM23F769i-DISCO that uses the USB peripheral as a device starting from a project generated with touchGFXDesigner.All seems to work when I am not enabling the DMA for the USB, but when I enable the DMA I...

JVALL.1 by Associate III
  • 778 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.