STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Since STM32Cube_FW_F7_V1.17.0 the HAL I2C Functions do not work the same. For a huge project that used to work with no issues on STM32Cube_FW_F7_V1.16.2 the I2C Data line goes low and the Firmware reports an HAL_I2C_ERROR_SIZE. Is there a known bug?

We are using a STM32F76ZI for a consumer device.The Firmware used to work fine with no errors.Since STM32Cube_FW_F7_V1.17.0 the I2C communication does not work all the time reporting random I2C Errors. The most common error is HAL_I2C_ERROR_SIZE that...

Interface IP camera with STM32

Hi all,Is it possible to capture image from an IP camera which is connected to an STM32 MCU via ethernet port? An external RAM can be added to handle the data traffic. Due to multiple reasons I cannot use a digital camera instead of an IP camera.Does...

SSala.3 by Associate III
  • 4940 Views
  • 7 replies
  • 0 kudos

How to check connection alive in LWIP?

Hello,I am using STM32H743 and imported the sample project LwIP_HTTP_Server_Netconn_RTOS. Is there anyway to indicate the TCPIP is still alive or not in case the ethernet cable is disconnected?Thanks

AFung.1 by Associate II
  • 6380 Views
  • 6 replies
  • 0 kudos

I have a question about the STM32G031. I want to confirm that the 28 pin package can be programmed using pins 18 and 19 with uart?

 according to the datasheet, I understand that PA11 and PA12 are mapped by default, which don't have USART TX/RX function, it should be changed to PA9 and PA10.AN2606 says that P9 and P10 can be usedDoes it mean that the bootloader automatically swit...

ECruz.2 by Associate
  • 1566 Views
  • 2 replies
  • 0 kudos

Resolved! UART_FLAG_TXE and UART_FLAG_TC not being set and reset during serial UART communication. How can I fix this?

Hello,I have made a custom board for the STM32G070KBT6 MCU to interface with other boards in an embedded project. I have added a mini–USB B connector to the PCB to communicate between the MCU and my computer. In the MCU, I am using one of the USART c...

HNass.2 by Associate II
  • 4364 Views
  • 5 replies
  • 0 kudos

udp client -at atm32h753 board ethernet-lwip

hii i have the stm32h753 nuclio board and i am trying to run udp client on the board and my pc will be UDP_SERVER , i am using udp_echoclient_connect() and  udp_echoclient_send()  functions, that are inside the files that is included in the project e...

abeba.1 by Associate III
  • 4982 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.