2022-11-14 5:41 AM
I need to change the UART parity from a FREERTOS task.
I also use interrupt per byte received.
Do I need to disable UART and interrupt before changing the parity?
I use LL API.
So what I do so far:
initialized_ = false; // Set initialized to false so interrupt handler will not touch flags which causes a hang
LL_USART_DisableIT_RXNE(uartHandle_); // Disable interrupt
LL_USART_Disable(uartHandle_);
auto parity = evenParity ? LL_USART_PARITY_EVEN : LL_USART_PARITY_NONE;
LL_USART_SetParity(uartHandle_, parity);
LL_USART_Enable(uartHandle_);
LL_USART_EnableIT_RXNE(uartHandle_); // Enable interrupt again
currentIndex_ = 0;
initialized_ = true;interrupt handler:
void Process()
{
if (!initialized_ || !LL_USART_IsActiveFlag_RXNE(uartHandle_) || !LL_USART_IsEnabledIT_RXNE(uartHandle_))
return;
// do stuff
}Am I overdoing it ? Code docs say nothing about how to change these parameters "on the fly" after the program is initialized and running, and I can't find any documentation what it takes to make the changes go into effect in a graceful way.
Thanks! :)
2022-11-14 6:26 AM
>>Am I overdoing it ?
Probably
With baud rates, etc, you just need to disable the UART (UE bit) whilst changing the settings.
However be aware of side effects. That it will change in-progress transmission/reception, and might flag errors/status that then need to be cleared, ie noise, framing, overrun, parity, etc.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.