STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Reading only zeroes from flash

Hello, i am trying to store adc calibration data in flash on my H7A3 project.Writing the data (64byte, flash addr 16byte aligned) is successful (at least i hope, since i get no errors), but when reading the same data back from flash via that same Ban...

95lux by Associate II
  • 390 Views
  • 3 replies
  • 4 kudos

Resolved! STM32H7 jump to application from bootloader

Hi everyone, I'm having trouble jumping to the app from the bootloader.The application is located here, writing doesn't give me errors. So I assume the problem is Jump.#define FLASH_USER_START_ADDR ADDR_FLASH_SECTOR_2_BANK1 Il main del bootloader è...

Giovanni3 by Associate III
  • 522 Views
  • 3 replies
  • 1 kudos

Resolved! Nucleo-H723ZG + FreeRTOS + LWIP

Hello everybody. I'm trying to make LWIP work on NUCLEO-H723ZG board, but I can't even get a ping response so far, even with static (DHCP disabled) network configuration. The project uses FreeRTOS (CMSIS API v2) and is created with MX tool. It seems ...

rzingler by Associate
  • 434 Views
  • 3 replies
  • 1 kudos

Resolved! FileX on QSPI files are not kept after reset

Hi,I’m working with a custom PCB based on an STM32H743BI and an external MT25TL01G memory device.To manage the data I’m using FileX + LevelX. I’m able to create the media, create directories, create files, write to them, and read them without issues....

JonConesa by Associate III
  • 406 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.