2026-02-12 7:05 PM - last edited on 2026-02-13 12:58 AM by Andrew Neil
Cannot build a very basic task i.e. blinking in built LED in STM32N657X0-Q Nucleo Board.
Please provide me the complete and step step procedure atleast how it happened and why.
Lots of issue and confusion occurs in this Board I don't know why but it occurs
2026-02-12 7:11 PM
Hi @Karan1511 ,
Have you had a chance to look at this: How to create an STM32N6 FSBL load and run - STMicroelectronics Community
2026-02-12 7:19 PM
2026-02-12 7:34 PM
Hello @Duc
I try each and every steps of both the the examples you show in that post, but nothing happened.
I have just one request please make a complete step by step procedure to atleast blink the LED using STM32N657X0-Q Nucleo Board and a post or videos
Thank you
2026-02-12 10:52 PM
Hello @Karan1511
To help you, the best place to start would be for you to explain what you are doing and how you are doing it.
For example:
1st Step:
Set the Nucleo-N657X-OQ board to DEV_BOOT mode (BOOT0 jumper in position 1 and BOOT1 in position 3). Are you able to compile and debug the existing project below?
https://github.com/STMicroelectronics/STM32CubeN6/tree/main/Projects/NUCLEO-N657X0-Q/Templates/Template
2nd Step:
As explained in the article mentioned by @Duc above, you must sign and program the FSBL binary produced in Step 1 into the board’s MX25 serial memory. Then you change the BOOT1 jumper to position 1 to enable Flash_Boot and press the RESET button.
Could you provide more details about what you are doing and what you are observing?
You can also refer to our official MOOC - STM32N6 demo workshop videos 4 and 5 should be usefull.
https://www.youtube.com/watch?v=3jnal51NBZQ&list=PLTJzs51NlEICI7ARAHOyUqMhTgJE0UFv0
Best regards,
Romain
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-12 11:36 PM
Yes I do the same as suggested in YouTube MOOC Demo Workshop and GitHub project.
Now, the cube programmer showing the core is locked.
Now, I have a special request you to please create a videos for the same step by step please just a special video using Nucleo board please 🥺
2026-02-13 5:30 AM
Hi @Karan1511
"Now, the cube programmer showing the core is locked."
You are trying to connect your board with STM32CubeProgrammer, can you confirm:
- What is the step on your side, do you want to flash your application in external Flash?
- Does Nucleo-N657X-0Q is in DEV_BOOT?
- Do you have enabled the External Loader MX25UM51245G_STM32N6570-NUCLEO.stldr ?
- Which STM32CubeProgrammer version are you using?
- Can you share a print screen error/warning message of STM32CubeProgrammer?
The video example already exists in MOOC STM32N6 demo workshop - 05 Booting process in practice.
and with the same example I mentioned. You just need to use the jumper BOOT1 to change N6 in DEV_BOOT or FLASH_BOOT instead the switch on the STM32N657-DK in the video. The process is the same.
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-13 5:34 AM
Here, I am sharing my project with all the codes, and please help me to figure it out.
https://github.com/Aditya-Goswami-01/STM32N657X0-Q-NUCLEO-BOARD
In this i upload, the everythings.
Just, i have a special request to @stmicro and all please make a separate special video for me, where we use all the three methods that are FSBL, APPLICATION and EXTERNAL Memory concept using STM32N657X0-Q Nucleo board please with each steps and faults take by us.
2026-02-13 5:44 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.