STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 NanoEdgeAIstudio

I call the following function:neai_classification(input_user_buffer, output_class_buffer, &id_class);When the program runs this function, it enters the following function:void HardFault_Handler(void) This is the first time to use, if you need other i...

HCYHCZ by Associate
  • 808 Views
  • 0 replies
  • 0 kudos

STM32G4 Errata 2.7.9 ADC trigger sequencing

ES0430 - Rev 8 - March 20232.7.9 An ADC instance may impact the accuracy of another ADC instance at specific conditionsHas anyone implemented this item listed in the Errata sheet for STM32G4 series for ADC section? It asks for:Ensure that conversions...

mitk by Associate II
  • 2028 Views
  • 3 replies
  • 0 kudos

How to use external SDRAM as an data memory?

I am using STM32H747I-DISCO board where the stack and heap memory allocated in SRAM , but I want to use external SDRAM as stack and heap memory, can any one please help me how to configure  external SDRAM as main data memory instead of SRAM.

How to use SDRAM for bss and data region?

I am using STM32H747I-DISCO board, I want to use external SDRAM for bss and data region and I called the SDRAM initialization function inside the SystemInit() function and I tried with the debugger point it will go to hard fault when debugger point h...

USBX CDC ACM on STM32F767 Nucleo board not working

I have spent over a week trying to get the USBX CDC ACM virtual com port to work on a STM32F7 family nucleo-144 board. I'm using an STM32F767 as a representative processor. I've tried multiple examples and approaches with no success.  The device enum...

tec683 by Associate III
  • 2903 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.