2023-12-18 11:09 AM - edited 2023-12-18 11:12 AM
I have callback ISR code (from UART) where I put in Semaphore put and other code with Threadx static implementation with stack (SRAM2), Semaphore get, etc. I placed two GPIO signals to measure the timing between put and get. I set the compiler to optimize for speed setting and used Logic Pro 8 to probe these two GPIO. The thread priority setting is 1.
I have other 3-4 treads running flashing LED but at a lower priority (around 10).
I found that STM32U5 while running on 160MHz to be 2.6uSec between semp put and semp get.
Microsoft spec claims 0.2uSec for 200MHz of something MCU. Have I missed something?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.