2024-05-21 2:03 AM
Is there anyone who experience this issue?
I use eeprom with I2C and USB OTG communication in STM32F407 discovery board. There is no common GPIO pin.
whenever I use USB OTG to write something in eeprom through I2C, USB and I2C looks disabled in same time.
I googled it and found there are similar issue but no solution at all.
is there any solution?
2024-05-21 2:57 AM
@Jimmy_LEE wrote:USB and I2C looks disabled in same time.
What do you mean by that?
What investigation/debugging have you done to find out what's going on ?
2024-05-21 4:47 AM
Are you sure there is no problem with interrupt management?
I felt that you were trying to perform long operations within the interrupt without seeing your code.
2024-05-21 11:01 AM - edited 2024-05-21 11:02 AM
Hi @Jimmy_LEE
Would you provide a minimum example to replicate this issue? you can check if it's applicable on specific I2C / OTG instance?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-24 5:55 AM
literally looks all function stop. No usb communication response to PC and no I2C response.
I have debugged them but I have no idea about this issue...
2024-05-24 5:59 AM
I think there is no problem with interrupt management. This is really weird. I have checked I2C interrupt couple of times..
2024-05-24 6:00 AM
You've marked this as solved - but it doesn't seem to be?
See this to un-mark a solution:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.