STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to transmit a printf to RTT Viewer.

Hi together,i am searching for a equivalent of the J-Link RTT-Viewer, on which i can display something for demonstration purposes. It is to simply demonstrate that i connection can work just like a in-built Segger J-Link. FYI: I am using a NUCLEO-C03...

STM32WB BLE

Hello ST,For our project, I want to broadcast a character with property "CHAR_PROP_BROADCAST" and I created it using the function aci_gatt_add_char(). But the function fails to add this character.In other case, when i change the property to "CHAR_PRO...

teja_111 by Associate II
  • 1052 Views
  • 1 replies
  • 0 kudos

ethernet delay between the requenst and response

HELLO,I'm using the stm32H755zit6 nucleo144 board, and I'm trying to communicate with the PC throw ethernet, all is working fine but the delay between the request and response is not enough for our application it's between 1ms  to 0.5ms and we need a...

belarbi by Associate II
  • 10077 Views
  • 5 replies
  • 2 kudos

Timer Frequency is unpredictable when using DAC

I am using STM32L496ZGT6P. I am using DAC along with DMA to generate voltage and frequency of my desired range. But I am unable to get hold of the frequency setting. Sysclk I set is 4Mhz. 20 is prescaler value, 4Mhz/20 = 200000.This is further divide...

SPI2 STM32H745

Hi everyone I can find help on how to connect SPI2 STM32H745. I have read the datasheet and did everything written on it.Please can someone help me 

fru999 by Associate III
  • 2804 Views
  • 4 replies
  • 0 kudos

Resolved! H5 1.2.0 and Cube 1.5 break ethernet

After updating Cube to v1.5 for my STM32H5 project (Nucleo-H563ZI), the ethernet stopped working except during the initial run after a load of the firmware with the debugger.  After a reset, either POR or via the debugger, pings to the board fail.  W...

robmilne by Associate III
  • 3688 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H745 SPI Accelerometer ADXL355

Hi everyone, I am trying to use an accelerometer with my STM32h745 board thought SPI.DO you have any idea where I can find library for thus accelerometers ?And how to use the SPI protocole with STM32H745 :)

fru999 by Associate III
  • 2005 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.