STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 firmware update (USB DFU) and encryption

HiI successfully got the USB DFU bootlader working in 2 hours.This one: https://www.youtube.com/watch?v=n_LDXOQHerUNow i would like to add some encryption to it with a time budget of couple of hours.I am already using python for USB DFU update.What i...

MK..1 by Senior
  • 3495 Views
  • 1 replies
  • 1 kudos

UDP packet loss

Posted on July 02, 2018 at 13:38Hi, im using stm32f7+ freertos+lwip (raw api). My system handles web server and udp data communication. My frame length is 572 bytes and my FPS is 40 (22880 bytes/sec) at start. When i increase the package number to 8...

0690X0000060C8qQAE.png

STM32U5G9 USB HUB+MSC transmission timeout

Hello,I want to test the read and write speed of U5 on the USB flash drive. I have made modifications to the demo (STM32U5G9J-DK2 \ Applications \ USBX \ Ux_Host_HUB_HID_MSC) so that I can observe the read and write speed.#define MASS_TEST_WR_LEN (64...

Xiang_0-1718349792318.png Xiang_1-1718349871401.png
Xiang by Associate II
  • 2667 Views
  • 4 replies
  • 0 kudos

USBC PD multiport TCPM debounce CC lines

Hi,I'm developing 3-port USB PD hub device with STM32 USBPD library. I have an issue with powering up device with a PD contract over USBC port when it has already plugged sinks on other ports.Investigation over I2C bus communication show that the iss...

vostrenkov_0-1718617535759.png

Resolved! Configure FatFs for 256 page size

Hello All,  I am planning to port FatFs on the IS25LP064A flash drive to communicate with my STM32H573ii over SPI. The FreeRTOS is running on STM32H573ii.According to the IS25LP064A datasheet, the maximum page size is 256 bytes. The total size of the...

paras by Associate
  • 1529 Views
  • 1 replies
  • 0 kudos

SPI DMA request triggered by Timer-compare

Hallo everyone,As engineer who started to explore the world of MCU's years after my retirement, I regularly encounter problems that puzzle me for some time. However, since I'm stuck for several days now, I decided to ask for assistance by this forum....

Scheme_Readout_CCD_w_SPI_ADC.png
FredS by Senior
  • 12247 Views
  • 25 replies
  • 0 kudos

HAL_ADCEx_EndOfSamplingCallback in DMA mode?

Is it possible to make HAL_ADCEx_EndOfSamplingCallback fire when ADC is running in the dual mode with DMA .More specifically: On a NUCLEO-H723ZG, the ADC is started by HAL_ADCEx_MultiModeStart_DMA() and ADC2 is a slave to ADC1. The ADC conversion is ...

pimaty by Associate
  • 1133 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.