STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! no Satel-VL53L8CX SPI example

Hi! I am developing a project which uses the satel-Vl53l8cx. I found many examples in I2C but none in SPI.The only one would be in VL53L8CX_ULD_driver_2.0.0 but this one was coded for the X-nucleo-Vl53l8A1.   A wiring is shown in AN5945 in SPI but in...

Antonin_m84_5-1720044853550.png Antonin_m84_6-1720044872426.png

Resolved! Nucleo STM32G431KB I2S

HelloI tried to implement I2S on the chip in question to send the data acquired by the on-board ADC (I tried both 8-bit and 12-bit) with DMA active on a curved buffer and half-word data size. The data should be read by an ESP32, connected to it on th...

AntoR by Associate III
  • 3169 Views
  • 4 replies
  • 2 kudos

Resolved! STM32U545REI6Q Bootloader GPIO config

AN2606 does a very good job of describing communication peripheral usage by the bootloader, but not so much GPIO pins.Can I get a description of how each of the GPIO pins on the ST32U545REI6Q is configured by the bootloader? This could be important i...

CSmit.4 by Associate II
  • 1595 Views
  • 2 replies
  • 1 kudos

Trying to programmatically get timer details

I use CubeMX to generate the set up code for clocks and peripherals in the STM32H7A3 I'm currently using for my current work.  I'd like to calculate the timer and low-power timer call back periods programmatically without having to type in magic numb...

magene_0-1720992964120.png magene_1-1720993221123.png
magene by Senior II
  • 3545 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.