STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32h7 ethernet tcp connection lwip

   /* add the network interface (IPv4/IPv6) with RTOS */ netif_add(&gnetif, &ipaddr, &netmask, &gw, NULL, &ethernetif_init, &tcpip_input); /* Registers the default network interface */ netif_set_default(&gnetif); if (netif_is_link_up(&gneti...

UDP communication on STM32H563ZI

I want to do UDP communication using ThreadX and NetXDuo on an STM32H563ZI.I searched for STM32Cube Examples and found a sample project for STM32H5, but because FW_H5_v1.3.0 does not exist, an error occurs.The following page is set up as an example o...

Nao05215 by Associate
  • 3323 Views
  • 5 replies
  • 0 kudos

Resolved! System Bootloader GO command doesn't work

I'm using stm32flash (https://sourceforge.net/projects/stm32flash) as my host on a raspberry pi. It's connected to the STM32H750 using I2C.Steps:Upload the code onto the STM32./stm32flash -a 0x4E -w stm32-blinky.bin -v -R /dev/i2c-1   stm32flash 0.6 ...

0693W00000HnsJIQAZ.png
dscdsc by Senior
  • 4307 Views
  • 3 replies
  • 0 kudos

Resolved! how do I get image end address from linker?

MCU : STM32F411CEU6 Hello everyone. I have an application in which I want to get image end address from linker. Here is a full context of what I want to do, I have a struct living in start of my image, which basically tells the bootloader usefull inf...

HZaib.1 by Associate III
  • 5796 Views
  • 5 replies
  • 1 kudos

Resolved! stm32f3xx_hal_def.h should be modified

IMHO in the file "stm32f3xx_hal_def.h" the section "Exported types" should be moved in front off section "Includes", because some of the types are used in the included files, but "stm32f3xx_hal_def.h" will not be reentered. It produces error like thi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.