STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Always SCL High, SDA Low In I2C

I am using the STM32F413ZH (T6U) model, there is no problem with this model, it is a very nice model in terms of features. However, problems start when I use the I2C protocol.When I checked the line with a logic analyzer, I saw that the SCL line is a...

Resolved! STM32F746 : SW not running well without debugger

Hi,I designed a sw on STM32F746 with STM32CubeIDE.Some functions work fine when I use the debugger (ST-LINK) but this same functions halts when I don't use the debugger !I play se sequence hereafter : - run the sw using debugger : execution ok- exit ...

ABITT.1 by Associate III
  • 3788 Views
  • 8 replies
  • 3 kudos

USBX Outputs Garbage

Still trying to get USBX to work, I can now get data out to Putty but it's all garbage and after each send it "dings" (very annoying).  I used the H5 example to get it working, last hurdle I guess.  Putty is set to 115200, 1 stop bit, 8 data bits jus...

kumaichi_0-1726157705752.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.