STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H750B - TouchGFX and Ethernet

Hi Using the following tools: TouchGFX Designer 4.24.0 CubeIDE 1.16.1 and CubeMx 6.11.0   I have attempted to build a system with ethernet capability.   I added the ethernet peripheral, LwIP compiled it without any errors, but the ethernet does not w...

Snag_15592871.png

Resolved! ST-Link Utility, Can not connect to target!

16:19:16 : Can not connect to target!Please select "Connect Under Reset" mode from Target->Settings menu and try again.If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.16...

zrtn_0-1710845376910.png
zrtn by Associate
  • 12880 Views
  • 5 replies
  • 1 kudos

GrEq audio library

Hello everyone, I am using a STM32H750 with STM32CubeExpansion_Audio_V1.1.1 and I am trying to use the Graphical equalizer library.This is what I've done: I have an aux audio signal that I'm sampling at 96Khz with a DMA's interrupt transfer every 1 m...

FCola.1 by Associate III
  • 2682 Views
  • 5 replies
  • 1 kudos

MQTT with TLS using STM32f767

I am using an STM32F767 with MQTT, and everything works without using TLS. But when I try to enable TLS, it fails to connect to the server because of a memory issue (calloc fails). I read other message boards that state that I need up to 60K of RAM t...

cleonb322 by Associate III
  • 1535 Views
  • 1 replies
  • 0 kudos

Resolved! LAN8742 Issue DuplexMode

Hello everyone, I'm currently using  Nucleo-H743ZI2  but this aim to go on a custum PCB. LWIP (2.1.2) is activated without FREERTOS and my TCP server is working. I'm also using HAL function with CubeIDE (1.16.1). And I'm using an Aruba 2530-8G switch...

AGP_29 by Associate III
  • 7156 Views
  • 9 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.