STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FATFS Failure with FreeRTOS

I am using the STM32H7B3I-DK for my project. I am trying to integrate uSD card usage with a touchgfx program. I have gotten a simple write to a file working on a non rtos project; however, when I use it in my project with RTOS I keep getting a hard f...

Resolved! SDMMC FATFS mount Hardfault

I have followed How to create a file system on a SD card using STM32CubeIDE the best I can using the STM32H7B3I-DK. With this board I do not see the DMA tab under SDMMC1, so I have skipped that. I am failing the f_mount(). I am using a touchGFX proje...

STM32H743 SPI DMA delay

Hello.I have a TIM3 configured to generate a PWM signal with frequency 1 MHz and duration 200 ns using CC1 channel. TIM3 also generates a DMA request on CC1.DMA1 is configured to transfer value 0xFFFF from AXI SRAM to SPI2_TXDR register, triggering t...

DS2_2024112683659.png

LPUART consumes extra 3mA while STOP2 mode

I'm using STM32WB55. The reference example is BLE_p2pServer with custom modifications. The power consumption of STOP2 mode ( by enabling CFG_LPM_SUPPORTED ) is around 6mA (board level), and it will be around 9mA after LPUART is enabled with RCC_LPUAR...

Charles_Li_0-1733297038620.png

Connect B-U585I-IOT2A to Azure IoT cloud

Hi Tech Support Team,I would like to connect the B-U585I-IOT2A board to Azure IoT cloud using STM32CUBE IDE.I am confusing on the setup steps.Should I go through the steps 1 and 2 then follow steps 3.b?Or just start with steps 3.b? And also, when bui...

bay_0-1714974852528.png bay_1-1714975031177.png
bay by Associate II
  • 8595 Views
  • 13 replies
  • 0 kudos

Resolved! SDCard FATFS f_mount always succeeds

I am using the STM32H7B3I-DK and followed How to create a file system on a SD card using STM32CubeIDE. I noticed that DMA options are not available on the SDMMC1 configuration tab, so I just skipped that step. The rest of the steps I followed. In FAT...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.