STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H723ZGT6 NetxDuo Custom Driver

In a project I created with STM32H723ZGT6, I am using the Wiznet W5500 Ethernet I/O Library. I decided to proceed with ThreadX and NetXDuo for my project. The issue is that I couldn't find an Ethernet driver for W5500 that works with NetXDuo. Where c...

AKULC.1 by Associate II
  • 1279 Views
  • 1 replies
  • 0 kudos

STM32H743iiK6 project with SD card not working

Hi,   I worked for last three weeks STM32H743iik6 project with SD card .SD card with SPI interface but I got FR_NOT_READY error.I have checked hardware connection.same code work in stm32f and stm32 l series.I don't know reason for stm32h series not w...

SK52 by Associate
  • 1644 Views
  • 2 replies
  • 2 kudos

Resolved! undefined reference to `netconn_set_sendtimeout'

I'm using the example for ModbusF429TCP from a GitHub repo for Modbus and get the following error: undefined reference to 'netconn_set_sendtimeout' I'm unfortunately still very new to STM32 and that's why I'm slightly overwhelmed nowGitHub repo is Mo...

krex by Associate
  • 2823 Views
  • 2 replies
  • 2 kudos

Resolved! STM32 USBD MIC AND STREAMING AUDIO

I am configuring USBD to turn the STM32F4 Discovery into a headphone, meaning it can play music through USB and transmit data from the PDM microphone to the computer. I have completed the music playback part, but I am now working on the recording par...

bacnk by Associate II
  • 2119 Views
  • 2 replies
  • 0 kudos

STM32 TIM CC IRQ and USART RXNE IRQ

Hi everyone,I’m working on an STM32C0 setup where TIM1 CH1 (Pin A) and UART RX (Pin B) are physically shorted together, and I’ve encountered some unexpected interrupt behavior. Specifically, the UART RXNE interrupt always triggers before the TIM1 Cap...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.