STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FREERTOS: How to enable osThreadIsSuspended ?

Hello Experts,I see that in cmsis_oc.c that the function osThreadIsSuspended is disabled. The variable INCLUDE_eTaskGetState is responsible for it.But how do we enable INCLUDE_eTaskGetState to 1 by default? I see in FreeRTOS.h header than the macro i...

ak52_0-1747306935740.png ak52_1-1747307040166.png
ak52 by Associate III
  • 1800 Views
  • 4 replies
  • 0 kudos

Resolved! AZURE RTOS Support H7S3

I have started looking at using the Azure RTOS package for my project but see it has since become Eclipse RTOS? Is STM supporting this RTOS anymore as I see the H7S3 Azure RTOS package was only updated seven months ago whereas the H7 branch as update...

Linduri by Associate II
  • 1299 Views
  • 1 replies
  • 1 kudos

Resolved! Stm32G491 I2C multimaster mode

Hi,I need to configure the I2C master on my STM32G491 to operate in a multimaster setup. It is currently connected to a slave device, but we also plan to connect another I2C master to the same bus. The slave device supports I2C multimaster communicat...

Make USB-to-Ethernet adapter

Hi,I intend to make an Ethernet to USB adapter by using a NUCLEO card (which already has the ports). The objective will be to communicate via USB between the nucleo and a PC, and from the nucleo to another PC. To develop this project I have a h563 an...

Guen1 by Associate II
  • 1866 Views
  • 4 replies
  • 0 kudos

WM8994 Audio Codec on STM32H747i-DISCO

Hello, I am having a difficult time with the WM8994 audio codec inside the STM32H747i-DISCO board, i am able to write to the registers and pass through analog audio through the speakers when avoiding any ADC and DAC signal routing but i am having a d...

Jpirsch by Associate
  • 1907 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.