STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IAP problem?

Hello everyone,I ran into a problem. First of all, I have two tablets: one with a bootloader and another without it. Tablet without bootloader works fine so its something bad in bootloader. I’m trying to plug in and unplug the power supply, and somet...

heyo_0-1752824790197.png
heyo by Senior
  • 1218 Views
  • 5 replies
  • 0 kudos

STM32H7 + LAN8742: No DHCP Request Observed

Hi,I'm using an STM32H7 board with a LAN8742 PHY, configured via STM32CubeMX.LwIP is initialized without RTOS, and Ethernet is in RMII mode. The main goal of this project is to receive data over UART and forward it via Ethernet.I want the STM32 board...

WhatsApp Image 2025-07-14 at 16.08.30_914e31a7.jpg WhatsApp Image 2025-07-14 at 16.08.30_c81398da.jpg
Matan by Associate
  • 1051 Views
  • 1 replies
  • 1 kudos

STM32H747I-DISCO: SAI DMA Returns Transfer Error

Hello,I am trying to fill a buffer from the on-board MEMS microphone using the BSP_AUDIO_IN_RecordPDM() function. However, execution pauses around HAL_SAI_Receive_DMA() and the BSP_AUDIO_IN_IRQHandler() is called. The stack trace is as follows:Checki...

miloa_0-1752192585335.png miloa_1-1752192658707.png
miloa by Associate III
  • 1720 Views
  • 11 replies
  • 0 kudos

ADDRERRF bit getting set on PKA init

Hello,I am trying to use the PKA module on a STM32U5 controller. I have configured the clock at 160Mhz and also initialized the Ring. However, when I try to initialize the PKA, it runs into ADDRERRF = 1, I was expecting ofcourse INITOK to be 1. Does ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.