2024-07-08 2:27 AM - last edited on 2024-07-08 5:07 AM by mƎALLEm
I have implemented microros on an stm32 nucleo f446re and wrote a publisher in it, while using default qos the messages published can't exceed the frequency more than one hertz even after removing the delay function.....Is there any way to increase the speed of the message publishing
this is the code of the thread
void StartDefaultTask(void *argument)
{
/* USER CODE BEGIN 5 */
// micro-ROS configuration
rmw_uros_set_custom_transport(
true,
(void *) &huart2,
cubemx_transport_open,
cubemx_transport_close,
cubemx_transport_write,
cubemx_transport_read);
rcl_allocator_t freeRTOS_allocator = rcutils_get_zero_initialized_allocator();
freeRTOS_allocator.allocate = microros_allocate;
freeRTOS_allocator.deallocate = microros_deallocate;
freeRTOS_allocator.reallocate = microros_reallocate;
freeRTOS_allocator.zero_allocate = microros_zero_allocate;
if (!rcutils_set_default_allocator(&freeRTOS_allocator)) {
printf("Error on default allocators (line %d)\n", __LINE__);
}
// micro-ROS app
rcl_publisher_t publisher;
std_msgs__msg__Int32 msg;
rclc_support_t support;
rcl_allocator_t allocator;
rcl_node_t node;
allocator = rcl_get_default_allocator();
//create init_options
rclc_support_init(&support, 0, NULL, &allocator);
// create node
rclc_node_init_default(&node, "cubemx_node", "", &support);
// create publisher
rclc_publisher_init_best_effort(
&publisher,
&node,
ROSIDL_GET_MSG_TYPE_SUPPORT(std_msgs, msg, Int32),
"cubemx_publisher");
msg.data = 0;
rcl_subscription_t subscription;
std_msgs__msg__Int32 sub_msg;
for(;;)
{
rcl_ret_t ret = rcl_publish(&publisher, &msg, NULL);
if (ret != RCL_RET_OK)
{
printf("Error publishing (line %d)\n", __LINE__);
}
msg.data++;
osDelay(10);
}
/* USER CODE END 5 */
}2024-10-30 9:03 AM
Hi, I'm new to working with Micro-ROS on STM32 microcontrollers. I've been experimenting with two Nucleo boards, the F446 and H723, as well as a custom F407 board. My development environment is Ubuntu 22.04 with ROS2 Humble, and the boards communicate via UART.
When I use OSDelay(10); I get the following communication rates by running ros2 topic hz /:
F446: 40 Hz , H723: 1 Hz
After adjusting to OSDelay(1); and generating the .c/.h files FreeRTOS.h, the rates changed to:
F446: 120 Hz , H723: 1 Hz
I'm not entirely sure why the H723 remains at 1 Hz, but 120 Hz on the F446 works well enough for my purposes. Hopefully, this may help.
2025-08-11 9:14 AM
Hi,
I am having the same issue. Can you help if you have solved it?
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.