STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H5 and EEPROM emulation with XCUBE-EEPROM

Hi, I'd like to have some feedback about the use of XCUBE-EEPROM library on STM32H563.Is it functionnal and reliable ? After digging into the code, i have few questions:   MPU_init() In the MPU_init() function there's a configuration  with no explana...

gh_rcl by Associate II
  • 1778 Views
  • 3 replies
  • 0 kudos

Cellular with in-modem IP stack

Hello,I am planning to build a cellular application using EC200 as my modem. I prefer to use in modem stack using AT commands due to memory constraint of my MCU. I have come across X Cube Cellular where it is mentioned this setting can be changed usi...

PSaga.1 by Associate III
  • 760 Views
  • 2 replies
  • 1 kudos

SD card formatting using fileX

Hi, It works, apparently a different microSd card works. however, it is strange that, DATALOG2 could write into the card. May i know how shall i perform sd card format function or what to fill up in the function?   Follow-up of the the topic below: S...

Resolved! "Ux_Host_DualClass" example on STM32N6570-DK

There is no test.txt file in my USB drive after the example is run.The board sends this log**** USB OTG HS Dual_Class Host **** USB Host library started. Starting Application Connect your HID or MSC Device USB Device Enumeration FailureTried to at...

ERROR by Senior
  • 1600 Views
  • 9 replies
  • 3 kudos

Resolved! PWM pattern changed after fixed no of cycles

Hi everyone,I am trying to generate sinewave using PWM mode of microcontroller.I am using Discovery Board having STM32F407 microcontroller. System clock and Timer clock are of 8MhzI am using two timers Timer1 for High Frequency switching (500Hz) and ...

PWM_response.jpg
AHayee by Associate II
  • 1093 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.