2025-08-23 4:23 AM - last edited on 2025-08-27 2:37 AM by Andrew Neil
There's a serious bug in G4's hal(version 1.6.1) library in spi dma function.
The problem is:
1, user calls HAL_SPI_TransmitReceive_DMA
2, after spi transmission finished, HAL will call HAL_SPI_TxRxCpltCallback
3, user calls HAL_SPI_Receive_DMA inside HAL_SPI_TxRxCpltCallback, and will fail in a chance.
The reason is:
1, HAL_SPI_TransmitReceive_DMA will start both Rx and Tx dma, and after transmission complete, HAL_DMA_IRQHandler will be triggered to set dma handler's state to ready and unlock dma handler;
2, If Rx dma complete first and trigger HAL_SPI_TxRxCpltCallback, user calls HAL_SPI_Receive_DMA in the callback, don't know why HAL will still start Tx dma which is still locked, that cause function to fail.
3, if Tx dma complete first, the scenario above will be fine. Unfortunately, these 2 simultaneously started dma(Rx & Tx) seem to complete in a random sequence (most of time Tx dma complete first) in my observation, in a rare case Rx dma will complete first which cause application to fail.
4, I compared with H7's HAL in HAL_SPI_Receive_DMA it only start Rx dma, that's why the same program runs ok in H7 platform.
The Workaround is:
add 2 lines below in HAL_SPI_TxRxCpltCallback:
__HAL_UNLOCK(hspi->hdmatx);
hspi->hdmatx->State = HAL_DMA_STATE_READY;
P.S.
If anyone recall I reported this porblem in a few month ago, at that time I just notice compile hal_dma.c as o1 will be somehow better, but unfortunately it's not the real cause.
STM32G4 HAL DMA start failed after software reset ... - STMicroelectronics Community
2025-08-25 3:48 AM - edited 2025-08-25 8:20 AM
Hello @TomZhu
Thank you for bringing this issue to our attention.
I reported this internally for HAL version 1.2.5.
Internal ticket number: 216230 (This is an internal tracking number and is not accessible or usable by customers).
2025-08-27 1:16 AM
Hi @Saket_Om
Sorry I'm using HAL version STM32Cube_FW_G4_V1.6.1. In the main thread I mixed up HAL version with DFP version.
2025-08-27 2:09 AM
@TomZhu wrote:1, user calls HAL_SPI_TransmitReceive_DMA
2, after spi transmission finished, HAL will call HAL_SPI_TxRxCpltCallback
3, user calls HAL_SPI_Receive_DMA inside HAL_SPI_TxRxCpltCallback, and will fail in a chance.
Why calling Receive in the callback?
Doesn't, TransmitReceive do both the transmit and the receive?
2025-08-27 7:27 AM
Hello @TomZhu
Have you tried setting the TX DMA interrupt priority higher than the RX DMA interrupt priority?
2025-08-28 12:11 AM - edited 2025-08-28 12:19 AM
Hi @Andrew Neil
To drive a populer imu sensor ICM-42688-P, we need first to read(using TransmitReceive function) its FIFO_COUNT register to determine how many bytes in its FIFO port, then generate SPI clocks(using Receive function) accordingly.
So the complete read behavior contains 2 phases, it's no matter the second phase using TransmitReceive or just Receive function, the important is first phase clock is predetermined(read FIFO_COUNT register), and the second phase clock is depending on the first phase result.
2025-08-28 12:41 AM
Hi @Saket_Om
No, I have not tried to change the interrupt priority. Because increase TX DMA interrupt priority may decrease the problem posibility, but can't resolve the problem. The product will fail on that point eventually.
Even worse, it's more difficult for us to reproduce the problem.
2025-08-28 3:40 AM
Hello @TomZhu
I cannot reproduce the issue from my side. Could you please describe the steps to reproduce the issue?
2025-08-28 9:26 AM - edited 2025-08-28 8:48 PM
Hello, @Saket_Om
Thank you for following up, I'm glad to share my procedure.
pseudo-code:
void test(void)
{
while (1)
{
if (read_flag) continue;
if (read_pin(drdy) == 0) // sensor data is ready, interrup pin was driven down
{
read_flag = 1;
write_cs(0); // pull down cs pin to start spi communication
HAL_SPI_TransmitReceive_DMA(); // read Fifo_Count register
}
}
}
void HAL_SPI_TxRxCpltCallback(hspi)
{
if (process_fifo_count() > threshold)
{
// read fifo port for x bytes according to fifo count, each fifo record is 20 bytes
HAL_SPI_Receive_DMA(fifo_count * 20); // this line will fail about 30 seconds after the application start, but I observed a few seconds or a few minutes survive time
}
else
{
// fifo count below threshold, terminate spi transmission. Since we start spi after interrupt pin, which means fifo already has enough data, this brunch should not occur.
read_flag = 0;
write_cs(1);
}
}
void HAL_SPI_RxCpltCallback(hspi)
{
// fifo data successfully received
// terminate spi transmission
read_flag = 0;
write_cs(1);
}
2025-08-28 9:23 PM
I traced into HAL_SPI_Receive_DMA, and find out it still calls HAL_SPI_TransmitReceive_DMA:
if ((hspi->Init.Direction == SPI_DIRECTION_2LINES) && (hspi->Init.Mode == SPI_MODE_MASTER))
{
hspi->State = HAL_SPI_STATE_BUSY_RX;
/* Check tx dma handle */
assert_param(IS_SPI_DMA_HANDLE(hspi->hdmatx));
/* Call transmit-receive function to send Dummy data on Tx line and generate clock on CLK line */
return HAL_SPI_TransmitReceive_DMA(hspi, pData, pData, Size);
}and fail point inside is:
/* Enable the Tx DMA Stream/Channel */
if (HAL_OK != HAL_DMA_Start_IT(hspi->hdmatx, (uint32_t)hspi->pTxBuffPtr, (uint32_t)&hspi->Instance->DR,
hspi->TxXferCount))Fail reason is tx dma is locked and hdmatx->State == HAL_DMA_STATE_BUSY.
These 2 states are cleared on tx dma's IRQ handler.
So the reasonable conclusion is tx dma's IRQ handler has not been lunched before HAL_SPI_Receive_DMA is called.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.