STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F401 ADC with DMA Example

I'm looking for an example to use as the starting point for a sensor data collector. In particular, an  STM32F401 ADC_MultichannelSingleConversion with DMA and software start. I found an example for the F11 that is based on the LL SDK. I then created...

Issue with FSBL Execution on STM32N6570-DK

Hello,I am working with the STM32N6570-DK and following the steps described in the following article to write the FSBL and application to flash and verify their operation:https://community.st.com/t5/stm32-mcus/how-to-create-an-stm32n6-fsbl-load-and-r...

nemoto by Associate
  • 1040 Views
  • 0 replies
  • 0 kudos

Resolved! STM32U5 - USBX memory defaults woefully small

TL;DR - adding USBX and the USB CDC device class to my STM32U5 TouchGFX project causes it to fail during initialization, because the default memory settings are woefully inadequate.I have a TouchGFX project running on an STM32U5G9J-DK2 using ThreadX....

usbx_init_failed.png
dmarks-ls by Associate III
  • 2346 Views
  • 4 replies
  • 2 kudos

Resolved! STM32H753 UsbX MSC + SDMMC DMA

Hi all,I'm currently working on a project using a STM32H753 in combination with the Azure RTOS UsbX to create a composite class USB device (CDC ACM + MSC). As a starting point for the MSC support, I'm using this STM github example:https://github.com/...

DZimm9_1-1748444380819.png DZimm9_4-1748445624362.png DZimm9_2-1748445167890.png DZimm9_3-1748445432939.png
DZimm.9 by Associate III
  • 3349 Views
  • 8 replies
  • 4 kudos

Resolved! STM32H7A3VGT: I2S Master with DMA

Hi,I am not able to output per I2S properly.1. I changed from a properly working driver for STM32F407 to this STM32H7A3VGTI had to learn, that the master clock is different as for the 407; here is always running (?) and the DMA did not work properly ...

Vmanne by Associate II
  • 697 Views
  • 2 replies
  • 1 kudos

Resolved! LWIP sends an arp request for himself

Hello,I am trying to set up  a UPD communication with a nucleo-H755ZI-Q board.Now I have the effect, that the lwip stack sends out an arp request for its own IP address.I double-checked the IP address and destination address to make sure they were co...

HiSt by Associate III
  • 992 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.