2025-09-02 5:19 AM - edited 2025-09-02 5:20 AM
Hi everyone,
I'm trying to interface an SD card over SPI with an STM32F411. However, I cannot even initialize it. My current sequence is:
Wait 20 ms after power-on.
Send 10 clock cycles with CS high.
Pull CS low and send CMD0 and wait for a reponse.
Instead, I only ever receive 0xFF instead of 0x01.
My SPI configuration looks like this:
Here is the relevant code:
MY_DEBUG_PRINTLN("Hello World");
uint8_t txBuf[6];
uint8_t resp = 0x00;
uint8_t dummy = 0xFF;
HAL_Delay(20);
MY_DEBUG_PRINT("Raw SD SPI test:\n");
// send 80 clocks with CS high
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_SET);
for (int i = 0; i < 10; i++) {
HAL_SPI_Transmit(&hspi2, &dummy, 1, HAL_MAX_DELAY);
}
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_RESET);
// CMD0 frame
txBuf[0] = 0x40;
txBuf[1] = 0x00;
txBuf[2] = 0x00;
txBuf[3] = 0x00;
txBuf[4] = 0x00;
txBuf[5] = 0x95;
// send command
HAL_SPI_Transmit(&hspi2, txBuf, 6, HAL_MAX_DELAY);
// wait for response
for (int i = 0; i < 30; i++) {
HAL_SPI_TransmitReceive(&hspi2, &dummy, &resp, 1, HAL_MAX_DELAY);
MY_DEBUG_PRINTF("resp = 0x%02X\r\n", resp);
if ((resp & 0x80) == 0) break;
}
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_SET);
MY_DEBUG_PRINTF("CMD0 resp = 0x%02X\r\n", resp);Output:
Hello World
Raw SD SPI test:
resp = 0xFF
... (30 times)
resp = 0xFF
CMD0 resp = 0xFF
On arduino if I execute the "same" code it works:
Serial.begin(115200);
while (!Serial) {}
Serial.println("Hello World");
uint8_t txBuf[6];
uint8_t resp = 0x00;
uint8_t dummy = 0xFF;
// SPI init
SPI.begin();
SPI.beginTransaction(SPISettings(100000, MSBFIRST, SPI_MODE0));
pinMode(SD_CS_PIN, OUTPUT);
digitalWrite(SD_CS_PIN, HIGH);
delay(20);
Serial.println("Raw SD SPI test:");
// send 80 clocks with CS high
for (int i = 0; i < 10; i++) {
SPI.transfer(dummy);
}
digitalWrite(SD_CS_PIN, LOW);
// CMD0 frame
txBuf[0] = 0x40;
txBuf[1] = 0x00;
txBuf[2] = 0x00;
txBuf[3] = 0x00;
txBuf[4] = 0x00;
txBuf[5] = 0x95;
// send the command frame
for (int i = 0; i < 6; i++) {
SPI.transfer(txBuf[i]);
}
// wait for response (max 30 tries)
for (int i = 0; i < 30; i++) {
resp = SPI.transfer(dummy);
Serial.print("resp = 0x");
Serial.println(resp, HEX);
if ((resp & 0x80) == 0) break;
}
digitalWrite(SD_CS_PIN, HIGH);
SPI.transfer(dummy);
Serial.print("CMD0 resp = 0x");
Serial.println(resp, HEX);
SPI.endTransaction();Output is:
Hello World
Raw SD SPI test:
resp = 0xFF
resp = 0x1
CMD0 resp = 0x1
I am running out of Ideas :(.
Solved! Go to Solution.
2025-09-03 4:58 PM
Hello Saket_om,
So in the end it randomly started working, after connecting it to an oscilloscope, the signals look similar. Maybe some jumper cable was broken?
Thank you!
2025-09-03 7:02 AM
Hello @estedebain
Did you try to check what happening on the bus using logic analyser? Is the SPI sending the CMD?
2025-09-03 4:58 PM
Hello Saket_om,
So in the end it randomly started working, after connecting it to an oscilloscope, the signals look similar. Maybe some jumper cable was broken?
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.