STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F09X Bootloader Mode.

We have a STM32F091 MCU board, it works, but we require to add bootloader function in for field update firmware.The BOOT0(PF11) is connect to GND via 10K resistor, so it will go to Flash Memory after power up, it does that (LED flash).I connect BOOT0...

Do I need to use VDDUSB pin on STM32L4?

Hi I am designing an application where the STM32L4 is connected to a PCs USB port. The board is always powered up by an external supply input, and not the PCs USB. Can anyone tell me if I have to use the VDDUSB pin on the STM32? I dont have to power ...

CMSIS linker files has error

Hi. I'm not sure is it a right place - my problem is more like an issue. I've downloaded STM32CubeF1 from here: https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-mcu-packages/st...

AOvch.0 by Associate
  • 1095 Views
  • 1 replies
  • 0 kudos

LowLevelLibrary without CubeMX

Hello, I'm an Italian guy so, please, forgive my terrible english. I want to use the LL library in the same way of the old SPL: without any other software like CubeMX. Is there a way to do that?Thanks,Davide

dcocc by Associate II
  • 2885 Views
  • 7 replies
  • 0 kudos

Nucleo-070RB USB DFU

Hi, I'm trying to enter the DFU mode over USB for the Nucleo-070RB. I have connected the USB DP and DM pins, and shorted the BOOT0 pin to Vdd. However, the device is not listed in DfuSe and device manager. In another post I read that for some 070 ver...

LStei by Associate
  • 675 Views
  • 0 replies
  • 0 kudos

STM32F4 Disc - receive data from accelerometer using SPI and transmit the data to bluetooth using UART with HAL

I'm having trouble using the HAL libraryies to send data I receive from the LIS3DSH accelerometer on the STM32F4 discovery to a HC-06 Bluetooth board.I can receive the data from the LIS3DSH fine and use STMStudio to check that the data is all streami...

MO'Su by Associate
  • 966 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.