2018-09-14 7:25 AM
Hi!
I have a project with a custom bootloader (I cannot change it), the issue I have is that my main app freezes after the jump from the bootloader.
I have a USART connection to debug it easily.
I know some Interruptions are set in the bootloader, so I tried to disable it at the beginning of my application, but still freezing.
I also know that the vector is in The RAM for the bootloader, and in the flash for my application. Could it comes from here?
Here is what I do in my main application:
=====================
__disable_irq();
SetupLeds();
SetSysClockTo72();
SetupTimers();
FLASH_Init();
Setup_USARTS();
Send_USART3("System Initialised, ENABLE IRQs\r\n");
__enable_irq();
__________________________
==> FREEZE HERE <==
------------------------------------
Send_USART3("LAUNCH !\r\n"); // never appears
while(1)
{
/* Applicative code */
}
=====================
I have my Faults_handlers set up (hardfault, memfault...) and none of them occurs...
I also tried to disable interruptions one by one like this:
=====================
for(uint8_t la=0;la<OTG_FS_IRQn;la++)
{
NVIC_DisableIRQ((IRQn_Type)la);
}
===================== Not successfull...
I try a lot of things but I dont know what to search, and how to make a diagnostic of it.
If whoever has an idea I am a taker...
Alexander
2018-09-14 8:29 AM
If you can't change the loader you need to understand it.
Are you sure it freezes and doesn't just fault? If you stop the debugger where is it?
Write a proper Hard Fault Handler, one that outputs diagnostic information so you know it ended up there.
Make sure your vector table location is reflected in SCB->VTOR
Where did you disable the interrupts generated by the loader?
Determine which peripherals/interrupts the loader enabled and services, and then deal with those in your app.
2018-09-17 1:20 AM
Thanks for your answer.
Write a proper Hard Fault Handler, one that outputs diagnostic information so you know it ended up there.
I set up all the faults handlers, My Hard_Fault_Handler is programmed to send through USART some informations on the issue, it is working:
uint8_t* BytePtr = (uint8_t)0x20002000;
*BytePtr = 0x5a; //generate hardfault IRQ
The HardFault handler is toggled if my hardfault test is before __enable_irq() , otherwise not...
Make sure your vector table location is reflected in SCB->VTOR If I plot SCB->VTOR it returns the rigth adress so I think its ok !?
Where did you disable the interrupts generated by the loader? Well I tried to stop it with :
for(uint8_t la=0;la<OTG_FS_IRQn;la++)
{
NVIC_DisableIRQ((IRQn_Type)la);
}
But I'm not sure it works. How should I do?
2018-09-17 9:12 AM
Ok I solved my problem:
I looked on the SCB->ICSR , the PENDSTSET bit was high:
I think systick interruptions was configured in the bootloader, and after the jump to my application the µC crash because there where no handlers in my code.
I just configured the SysTick_Handler() and it solved my problem, I'll try to disable the interruption to be cleaner.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.