2018-09-17 10:05 AM
I'm having trouble using the HAL libraryies to send data I receive from the LIS3DSH accelerometer on the STM32F4 discovery to a HC-06 Bluetooth board.
I can receive the data from the LIS3DSH fine and use STMStudio to check that the data is all streaming ok.
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
UNUSED(GPIO_Pin);
//SPI Recieve**********************
// 1. Bring Slave Sel Low
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_RESET);
// 2. Transmit register+0x80 (set MSB bit high -read mode)
spiTxBuf[0] = 0x29|0x80;
HAL_SPI_Transmit(&SPIHand, spiTxBuf, 1, 50);
// 3. Receive Data
HAL_SPI_Receive(&SPIHand, spiRxBuf, 1, 50);
// 4. Bring Slave Sel High
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_3, GPIO_PIN_SET);
HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12);
}Now, I want to take the data I receive from HAL_SPI_Receive and pass it to a HAL_UART_Transmit function to send the data to a HC-06 Bluetooth chip. I've checked that my UART code is working fine. I can send strings no problem, and check that I receive them properly in a Bluetooth terminal.
But I can't figure out how to send the spiRxBuf. All I am doing so far is adding the following line to the end of the HAL_GPIO_EXTI_Callback function. I do not receive any data using this code.
HAL_UART_Transmit(&UartHand, spiRxBuf, 1, 20);Can someone please tell me how to do this?
Thanks,
Mark
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.