STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with HAL_UART_Transmit_DMA

I’m using the STM32F401RET6 board, collecting data from a USB accelerometer at 16 kHz.I wanted to verify that the data is actually being collected at 16 kHz, and then run an FFT to compare it with previously collected PC data. To do this, I need to t...

Para033 by Associate
  • 1503 Views
  • 4 replies
  • 1 kudos

F103C8 USART DMA Issue

Hi, I'm having the following issue with the F103C8 USART DMA.After reset, sometimes the USART DMA Receive doesn't work. It doesn't happen every time, but it happens about once every 10 resets. HAL_UARTEx_ReceiveToIdle_DMA(&huart1, (uint8_t *)RxDataUs...

asttekin by Associate II
  • 563 Views
  • 3 replies
  • 1 kudos

Resolved! Simple ISR for DMA

I'm losing my mind a little, because this seems like it should be a simple task. I have configured my I2C module to enable DMA and interrupts: I can confirm that my call to HAL_I2C_Master_Transmit_DMA returns OK. I can also confirm that the generate...

avidroneg_0-1760975095854.png
avidroneg by Associate III
  • 849 Views
  • 4 replies
  • 3 kudos

Resolved! STM32N6 DK ETH problem

I use STM32Cube FW_N6 V1.2.0 to create an FW to run a web server on the DK board. I figured out that I can not talk to the PHY chip to read the PHY ID. I compared the code with another example that ST released and figured out that these codes are mis...

AliR by Associate
  • 616 Views
  • 2 replies
  • 1 kudos

DMA2D minimum width requirement?

Hello,I'm using a H743 with the DMA2D device in RegToMem mode.  Generally it seems to work for larger images, but I've been trying to fill a small rectangle (5 x 60) pixels, and I was expecting 300 write pulses.  Instead, I'm getting 480 pulses (8 x ...

matt-crc by Senior III
  • 516 Views
  • 2 replies
  • 0 kudos

CAN RX ring buffer interrupt

I am simulating messages to be received via CAN on the STM32F0xx series uC. The hardware FIFO does not overflow as I have activated the overflow interrupt and checked the FIFO level, which never exceeds 1. The current implementation consists of a 128...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.