2025-10-19 6:40 PM - last edited on 2025-10-20 4:19 AM by mƎALLEm
I use STM32Cube FW_N6 V1.2.0 to create an FW to run a web server on the DK board. I figured out that I can not talk to the PHY chip to read the PHY ID. I compared the code with another example that ST released and figured out that these codes are missing on HAL_ETH_MspInit
__HAL_RCC_ETH1MAC_CLK_ENABLE();
__HAL_RCC_ETH1RX_CLK_ENABLE();
__HAL_RCC_ETH1TX_CLK_ENABLE();
after adding this to my MSPInit function problem was solved!
I wonder if this is a bug in this package or if I need to set it in the CubeMX settings?
Solved! Go to Solution.
2025-10-20 6:21 AM - edited 2025-10-20 6:22 AM
Hello @AliR,
This issue has already been escalated to the relevant team for resolution and is being tracked internally under ticket number 213570. Thank you again!
Best regards,
2025-10-20 3:34 AM
Hello @AliR, and welcome to ST Community!
Thank you for reporting this. I will investigate this and get back to you with feedback.
Best regards,
2025-10-20 6:21 AM - edited 2025-10-20 6:22 AM
Hello @AliR,
This issue has already been escalated to the relevant team for resolution and is being tracked internally under ticket number 213570. Thank you again!
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.