2025-10-15 2:40 PM
Hello,
I'm using a H743 with the DMA2D device in RegToMem mode. Generally it seems to work for larger images, but I've been trying to fill a small rectangle (5 x 60) pixels, and I was expecting 300 write pulses. Instead, I'm getting 480 pulses (8 x 60 pixels)???. Is there a weird requirement that the width of the fill has to be a multiple of 8? I don't remember seeing such a requirement in the datasheet.
thanks
Matthew
2025-10-15 6:21 PM - edited 2025-10-15 6:33 PM
More info....
If I transfer a small image (5x1) pixels, it writes (8 x 1 pixels) FAILED
If I transfer a small image (8x1) pixels, it writes (8 x 1 pixels) <<< this worked
If I transfer a small image (4x1) pixels, it writes (4 x 1 pixels) <<< this worked
If I transfer a small image (1x1) pixels, it writes (4 x 1 pixels) FAILED
If I transfer a small image (12 x 1) pixels, it writes (12 x 1 pixels) <<< this worked
If I transfer a small image (11 x 2) pixels, it writes (14 x 2 pixels) <<< FAILED weird result
if I transfer a small image (12 x 2) pixels, it writes (12 x 2 pixels) <<< this worked
The DMA2d hardware seems very flakey and unpredictable. After running these tests, I thought there was a min width of 4 pixels, but the (11 x 2) image blew that pattern. (and yes it is repeatable).
Does anyone have any ideas? I know the H743 has over 80 pages of errata's, if I migrate to another processor (ie the new N657), will the DMA2D work on that version of silicon?
Test code:
/*******************************************************************************
* LCD Fill - fill rectangle with a single color
******************************************************************************/
void LCD_ILI9488_Fill(uint16_t x1, uint16_t y1, uint16_t x2, uint16_t y2, uint32_t color) {
LCD_ILI9488_SetWindow(x1, y1, x2-1, y2-1);
HAL_StatusTypeDef ret;
if(HAL_DMA2D_Start(&hdma2d, color, 0x64000000, (x2-x1), (y2-y1)) != HAL_OK) {
syslog(SYSLOG_ERROR, "DMA start error");
}
ret = HAL_DMA2D_PollForTransfer(&hdma2d, 50);
if (ret != HAL_OK) {
syslog(SYSLOG_ERROR, "DMA2D poll error");
while(1);
}
2025-10-20 3:08 AM - edited 2025-10-20 3:08 AM
Hi @matt-crc,
We've noticed you opened a case to our ST Online Support Team for additional assistance on this.
They'll contact you directly on this.
I will close this conversation to avoid the duplication of effort of our colleagues.
Best regards,
Lina
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.