STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_SPI_Transmit takes too long

Posted on May 22, 2017 at 19:51 Hi guys, I am working with the STM32L486 using the CubeMX tool and running into some SPI issue that I can't seem to figure out (I am new to ST chipsets btw). Specifically the HAL_SPI_Transmit routine takes to long...

0690X000006072dQAA.png
e d by Associate II
  • 5910 Views
  • 10 replies
  • 0 kudos

File transfer through Ethernet

Hi all,How to transfer file through server to target board using Ethernet ?I'm using STM32F429 Nucleo-144 board, currently done with STM32F4xx Webserver Demo ( Based on the lwIP TCP/IP stack ). Based on this server demo how transfer file server to ta...

chum by Associate II
  • 2667 Views
  • 3 replies
  • 0 kudos

How to use I2C to read GPIO pins on STM3241G-Eval

Hi,I have STM3241G-Eval board and I'm trying to learn things.Did some LED blinking and now trying to get in to the I2C world.So I created a project with STM32CubeMX and initialized all peripherals with their default Modes.I enabled FREERTOS and gener...

0690X0000088KIcQAM.jpg 0690X0000088KKxQAM.jpg 0690X0000088KLWQA2.jpg 0690X0000088KMFQA2.jpg
valtteri by Associate II
  • 1114 Views
  • 0 replies
  • 0 kudos

USB CDC Change Device name

Posted on April 28, 2017 at 12:29Hey,i use the STM32F4 USB CDC (generate by CUBEMX(v.4.20)) and want change the shown name in the Device Manager.I change these lines but nothing change in the device manager.&sharpdefine USBD_VID     1155&sharpdefine...

HAL_SPI_Transmit on F0, F1, F4, F7

Hi!I have module for transmit dates to SPI Interface.Data is - pointer to data buffer uint8_t.In F1 & F4 all will be ok.But in F0 & F7 modules will send *((uint16_t *)pData) (see modules below)Program for F1 or F4 will not work on F0 & F7.Where error...

VLev by Associate II
  • 6250 Views
  • 17 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.