STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_Receive_IT usage

I'm having trouble understanding correct usage of the HAL UART functions to receive incoming bytes. The function assumes you know the byte count in advance. I would expect a receive function to respond to receive buffer full,empty and maybe half full...

Documents on CAN Hal libraries.

Hi,I'm working with a STM32F446, on a CAN Bus system. My question is on PDF documents: there is a new version of the document UM1725 (or other) where find the new complete set of functions (like HAL_CAN_AddTxMessage(..)) ? . The only way is read the ...

STM32F4x STMicroelectronics Virtual COM Port is properly installed but can't start, error ''This device cannot start. (Code 10)'' WIN7 64 (FIXED!)

Hi, in case someone else have the same issue which is Installed the WIN7 64Bits USB Virtual COM Port cant't start with Code 10,   Software and Library versions, I am using Firmware Library "STM32Cube_FW_F4_V1.24.0"STM32CubeMX V5.0.1 and STM32Cube V1....

0690X0000088SkFQAU.png 0690X0000088SkAQAU.png 0690X0000088SlDQAU.png 0690X0000088SmLQAU.png

How to use DMA?

Hello togetherI'm brand new to the field and I'm just starting getting used to it. So please forgive me "stupid questions" :)The ultimate goal of my task is to continuously analyze sensor data by means of an STM32 (currently F44RE Nucleo board for te...

YHaag by Associate
  • 687 Views
  • 0 replies
  • 0 kudos

STM32 F407 ethernet IP problem

Hi,I created C code for STM32 F407VE ethernet project using STM32 CubeMX. Ethernet leds are blinking but when I ping boards static IP(DHCP closed) from my PC no response is coming. I saw a similar post suggesting to change PHY address in Cube MX from...

Murkm by Associate
  • 733 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.