STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 talking to USB Peripheral with 3 Endpoints

Hi,I'm developing a new project that will use a GSM module. On the PC, this presents as three (3) Endpoints e.g. COM5, COM6 & COM7. I need to communicate with the GSM module on at least two of the three endpoints using the AT command protocol.Will a ...

NW27 by Associate III
  • 1358 Views
  • 2 replies
  • 0 kudos

I'm trying to use FATFS library with my SPI-Flash. How can I format it in a right way. I'm using 16Mb flash. W25q16. It has 64 Blocks, each Block has 8 sectors. Total 512 sectors, each sector has 16 pages, each page has 256 Byte.

I traced the code flow and I found that the SPI flash should be formatted.I used an SD-Card and traced the code while it is mounted and knew that it searches in sector 0 for the record signature and the pointer to the partition sector. Then it reads ...

MShafiee by Associate
  • 3254 Views
  • 2 replies
  • 0 kudos

Unable to Initialize Uart (HAL_UART_Init())

Hi everyone,I want to start using the H743ZI serial communication with an hyperterminal software but i am not able to compile my project. I am using the STM32Cube_FW_H7_V1.3.0 UART POLLING example as a reference but everytime i try to compile my proj...

MEsco by Associate II
  • 5456 Views
  • 8 replies
  • 0 kudos

FreeRTOS good practices

Hello,I don't really have a problem, but I'm asking myself questions and I didn't succeed in synthesizing them and find answers on Google.Problem 1:Several tasks want to use the same peripheral, lets say SPI bus for example. What is the best way to p...

Bootloader cannot flash hex files with shorter lines

Hi,we have a hex file coming from GCC which we cannot flash onto the MCU with our own flashing tool (F412 and L471 tested).While investigating, we found that after a shorter line all writing seems to fail silently (still receiving ACK).In the picture...

FS.1 by Associate III
  • 2940 Views
  • 5 replies
  • 0 kudos

Issues with SPI using HAL

Hi,I'm new to using HAL, and I'm having several issues with setting up the SPI.I'm using SPI 1 on an STM32F429ZGT6, and using KEIL as my IDE.I've just tried initializing SPI 1 by configuring GPIOA Pins 5, 6 and 7 for their SPI Alternate functions.I s...

EDaws.1 by Associate II
  • 5446 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.