STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem entering USART1 boot

We are using an STM32L151RE.We have problem entering USART1 boot on some of the boards. We set RESET low, BOOT0 high, then set RESET high. Then we send 0x7F on USART1 and get 0x79 as reply (on the working boards). The non working boards does not repl...

0693W000001sFpaQAE.png
MSipo by Senior II
  • 2443 Views
  • 7 replies
  • 0 kudos

Resolved! STM32F7xx.h: Strange USB_HS_PHYC_LDO_ENABLE definition

Hello,STM32Cube_FW_F7_V1.16.0 Drivers/CMSIS/Device/ST/STM32F7xx/Include/stm32f730xx.hdefines#define USB_HS_PHYC_LDO_ENABLE_Pos              USB_HS_PHYC_LDO_DISABLE_Pos#define USB_HS_PHYC_LDO_ENABLE_Msk              USB_HS_PHYC_LDO_DISABLE_Msk#define ...

USB HOST on stm32f469 and Composite Device

I have custom board on stm32f469. And I try add to HAL HID library my USB device. But I have some problem.Device have 2 interfaces. 1 endpoint in first and 2 endpoins in second (interface). In this case USBH_HID_GetHIDDescriptor give me descriptor, b...

USB Mass Storage bridge to monitor USB traffic

HiI have stm32f446re nucleo. Is it possible to make one USB traffic monitoring bridge using it?(USB Storage or SDCard) <-----STM32-----> ComputerI am trying to do is to make one monitor to see what content is getting accessed from the computer from t...

SSune.1 by Associate II
  • 5426 Views
  • 13 replies
  • 0 kudos

Hello everybody! I've got a development board NUCLEO-H743ZI2. I try to study USB using STM32CUBEMX. I always get an error 43 in my windows PC after reconnecting. Can anybody say to me what I've do wrong?

 I configured clock configuration and USB CDC with default settings without using VBUS. In main() i try to sent a message to PC using function CDC_Transmit_FS which was generated CUBEMX. First connection to PC is successful and i got my messages. Aft...

AAA.1 by Associate
  • 610 Views
  • 0 replies
  • 1 kudos

STM32G071 - Problem with rand() and random() functions always returning 0 in a FreeRTOS thread but OK in main().

I have an STM32G071 running FreeRTOS CMSIS v2 compiled with STM32CubeIDE. In one of the threads I want to generate a pseudo-random number. (I don't need anything sophisticated and the STM32G071 doesn't have an RNG anyway; pseudo random is absolutely ...

SSton.1 by Associate III
  • 7281 Views
  • 6 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.