2020-07-08 9:46 PM
Hi,
I'm developing a new project that will use a GSM module. On the PC, this presents as three (3) Endpoints e.g. COM5, COM6 & COM7. I need to communicate with the GSM module on at least two of the three endpoints using the AT command protocol.
Will a STM32 talk to three endpoints?
I started with a STM32L476RG but ran out of peripherals etc, so have moved to a STM32F767V for further expansion.
My idea was to have a SD card on the STM32 that the PC could connect to via the USB_Device & Mass Storage Class but I guess this would be a problem now. Combination USB_Host and USB_Device doesn't work.
I could have a 2nd STM32 that talks to the GSM module via the USB and then talks to the above STM32F767 via SPI?? This way I keep the SD to PC USB interface operating.
Thoughts?
Thanks, Neil.
Solved! Go to Solution.
2020-07-09 4:29 PM
Thanks.
2020-07-09 12:57 PM
> GSM module
Based on the device/configuration descriptors, what class is device and the interfaces? It's quite possibly not standard CDC ACM, and that's a showstopper (and there's a custom driver in PC).
The 'F7 has two OTG modules, one of them can be host and the other device.
JW
2020-07-09 4:29 PM
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.