2024-08-27 2:59 AM
I have a Nucleo F746ZG board and I've implemented a small UDP echo server in LwIP standalone mode. (No RTOS)
If I hit 'debug' and as soon as the code stops on the first instruction hit 'continue' then it works perfectly.
If however I just run the code, (no debugging) or reset the board it does not work. It sits in a loop patiently waiting for a DHCP address. I know this because I use the three LEDs to show status.
Here is my main loop code:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* Enable the CPU Cache */
/* Enable I-Cache---------------------------------------------------------*/
SCB_EnableICache();
/* Enable D-Cache---------------------------------------------------------*/
SCB_EnableDCache();
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_USB_OTG_FS_PCD_Init();
MX_LWIP_Init();
/* USER CODE BEGIN 2 */
HAL_GPIO_WritePin(LED_GREEN_PORT, LED_GREEN_PIN, GPIO_PIN_RESET);
HAL_GPIO_WritePin(LED_BLUE_PORT, LED_BLUE_PIN, GPIO_PIN_RESET);
HAL_GPIO_WritePin(LED_RED_PORT, LED_RED_PIN, GPIO_PIN_SET);
while(dhcp_supplied_address(&gnetif)==0) {
ethernetif_input(&gnetif);
sys_check_timeouts();
HAL_Delay(100);
}
HAL_GPIO_WritePin(LED_BLUE_PORT, LED_BLUE_PIN, GPIO_PIN_SET);
udpServer_init();
HAL_GPIO_WritePin(LED_GREEN_PORT, LED_GREEN_PIN, GPIO_PIN_SET);
HAL_GPIO_WritePin(LED_RED_PORT, LED_RED_PIN, GPIO_PIN_RESET);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
ethernetif_input(&gnetif);
sys_check_timeouts();
}
/* USER CODE END 3 */
}
As you can see it's reasonably straightforward. I turn on the RED led, wait for a DHCP address (pumping the LWiP timeouts as required) and when it comes in switch on the BLUE led, and then when everything is running, switch off the RED and turn on the green.
In debug this works fine, even without stepping.
In run time it stops after the red led comes on.
I'm guessing timing issue, or HAL_Delay() is hanging up?
Any ideas?
Solved! Go to Solution.
2024-08-27 7:59 AM
Hello @KMill,
It appears that is a timing or synchronization issue. Debug mode can introduce additional delays that allow certain components to initialize correctly. Please try adding a delay after the initialization of the peripherals.
With Regards,
2024-08-27 7:59 AM
Hello @KMill,
It appears that is a timing or synchronization issue. Debug mode can introduce additional delays that allow certain components to initialize correctly. Please try adding a delay after the initialization of the peripherals.
With Regards,
2024-08-27 8:08 AM
Hi @ASEHST
Thanks for your suggestion.
If I add 1800ms of delay after SystemClockConfig() then it all works.
I tried 1500ms too, but it was too little. I would love to understand what is happening here, but for now I'll just include that delay. I have placed it inside the USER CODE BEGIN SysInit block.
Thanks again.
2025-03-04 12:22 AM
@KMill wrote:I would love to understand what is happening here
Yes, that would be better than just inserting an arbitrary, "blind" delay!
See also:
2025-03-26 5:47 AM - edited 2025-03-26 5:51 AM
@ASEHST wrote:It appears that is a timing or synchronization issue.
Indeed.
So far, (at least) three people have been bitten by it - on NetX-Duo as well as LwIP:
https://community.st.com/t5/stm32-mcus-embedded-software/stm32f767-lwip-tcp-client/m-p/777886
Seems that someone should look into this, and find what's actually going on - so that people don't just have to rely on arbitrary delays.
2025-05-15 2:04 AM
@KMill wrote:I would love to understand what is happening here,
Did you ever look into that?
Perhaps take a look at the two posts by @Guillaume K in this thread:
https://community.st.com/t5/stm32-mcus-embedded-software/stm32f767-lwip-tcp-client/m-p/778561
do they address your issue?
2025-05-15 2:27 AM
Hi @Andrew Neil and thank you.
Yeah I've been following that thread too.
Unfortunately, because the delay that fixes the issue is before LWiP is even initialised, any fix would maybe need to be inside the HAL or 3rd Party code itself. Thus, could get overwritten in any updates.
I thihk it's OK to call it a bug in the LWiP implementation, or the HAL somwwhere. ;)
And I think it's ok in my instance to use the delay after the system clock init, as this works for me, and the extended boot time is not an issue. Other's might need a more elegant solution ;)
Cheers!
2025-07-07 8:17 AM
Hello @KMill ,
During the initialization process, the ETH MAC must be configured with the correct Ethernet link speed and duplex mode after the auto-negotiation process is completed, which can take up to few seconds (see the API HAL_ETH_SetMACConfig).
To resolve the issue, a call to the API Ethernet_Link_Periodic_Handle in your both loops (dhcp_supplied_address & main) must be added.
This API will periodically polls the PHY status and updates the MAC configurations if any changes occur to the Ethernet link.
An example can be retrieved in "STM32F769I_EVAL\Applications\LwIP\LwIP_HTTP_Server_Raw" application in STM32CubeF7 v1.17.0 package.
Note: There is no need to add an additional HAL_delay().
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.