STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 HAL_Delay twice as long

Hello,I'm here on H753, external clock, CPU clock configured to 400MHz. Setup code is generated by CubeMx.If I execute a HAL_Delay() takes twice the time as expected, e.g. 2ms instead 1ms. I checked via GPIO toggle with a scope.The MCO output is corr...

regjoe by Senior II
  • 2128 Views
  • 5 replies
  • 2 kudos

Resolved! USB C PD Try.SRC and Try.SNK

I can't find Try.SRC or Try.SNK features for DRP devices in ST's USB C Power Delivery Stack (USBPD Core). Did I miss something?If it is not in the stack yet. Is ST planning to integrate this feature? What timeline are we looking at?Is it easy to impl...

abtq by Associate III
  • 1087 Views
  • 1 replies
  • 1 kudos

Resolved! SDIO with STM32U575

Hello everyone! I'm working on a project using an STM32U575 microcontroller, and I need to manage an SD card (read, write, etc.) via SDIO in 1-bit mode, but without using FreeRTOS. I noticed that FatFs is not natively supported for this MCU in STM32...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.