2025-07-07 2:21 AM - edited 2025-07-07 5:07 AM
I'm attempting to use I2S to drive the WM8978 for audio recording (the SAI pins are already occupied, so please don't suggest switching to SAI). I've ported the well-tested WM8978 driver code from the F4 series and configured I2S DMA to receive data. However, I haven't been able to receive audio data—there's only clean background noise. I've tested the waveforms at the I2S interface, and here's how I've configured I2S in my code:
<i2s config>
hi2s3.Instance = SPI3;
hi2s3.Init.Mode = I2S_MODE_MASTER_RX;
hi2s3.Init.Standard = I2S_STANDARD_PCM_SHORT;//I2S_STANDARD_PHILIPS;
hi2s3.Init.DataFormat = I2S_DATAFORMAT_16B;
hi2s3.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
hi2s3.Init.AudioFreq = I2S_AUDIOFREQ_8K;
hi2s3.Init.CPOL = I2S_CPOL_LOW;
hi2s3.Init.FirstBit = I2S_FIRSTBIT_MSB;
hi2s3.Init.WSInversion = I2S_WS_INVERSION_DISABLE;
hi2s3.Init.Data24BitAlignment = I2S_DATA_24BIT_ALIGNMENT_RIGHT;
hi2s3.Init.MasterKeepIOState = I2S_MASTER_KEEP_IO_STATE_DISABLE;
<wm8978 config>
bsp_InitI2C();
wm8978_Init();
WM8978_ADDA_Cfg(0,1);
WM8978_Input_Cfg(1,0,0);
WM8978_Output_Cfg(0,1);
WM8978_MIC_Gain(46);
WM8978_LINEIN_Gain(5);
WM8978_I2S_Cfg(3,0);//PCM Format
MX_I2S3_Init();
<Callback>
void HAL_I2S_RxCpltCallback(I2S_HandleTypeDef *hi2s)
{
if(hi2s->Instance == SPI3)
{
current_buf_flag = pcm_buf_flag;
pcm_buf_flag = !pcm_buf_flag;
HAL_I2S_Receive_DMA(&hi2s3, pcm_data[pcm_buf_flag], PCM_SIZE/2);
AsrEventFlag = true;
}
}
<main while>
while (1)
{
if(AsrEventFlag)
{
AsrEventFlag = false;
HAL_GPIO_TogglePin(GPIOE,GPIO_PIN_2);
HAL_UART_Transmit_IT(&huart5,(uint8_t*)pcm_data[current_buf_flag],PCM_SIZE);
}
}
The measured MCLK is 1.024 MHz, and WS, SCK, and SDI are all around 8 kHz, but I still can't receive audio data correctly. Why aren't there any I2S examples for the H7? Can someone who has used the H7's I2S interface help me out?
2025-07-07 6:45 AM
Hello @JfSDK
Please refer to the example I2S_Audio
2025-07-07 7:23 AM
Hello @JfSDK
I recommend checking out this post for the SAI & I2S in STM32H7 : https://community.st.com/t5/stm32-mcus-products/stm32h723-i2s-or-sai/td-p/681752#:~:text=Given%20that%20the%20SAI%20can,advanced%20features%20in%20the%20future.&text=For%2032%2Dbit%20audio%20samples,for%2032%2Dbit%20audio%20frames.&text=I%20like%20the%20SAI%20more,with%20internal%20signals%20than%20....
You can refer to the STM32CubeF4 firmware package for I2S examples and applications. It contains ready-to-use I2S configurations and sample projects that demonstrate how to implement I2S communication. If needed, you can adapt and port these examples to your specific STM32 board .
you can find in ST.com by downloading STM32Cube package :
- /Projects/STM324xG_EVAL/Examples/I2S/I2S_Audio
- /Projects/STM324xG_EVAL/Applications/USB_Device/AUDIO_Standalone
- /Projects/STM32F401-Discovery/Applications/Audio/Audio_playback_and_record
- /Projects/STM32F4-Discovery/Applications/Audio/Audio_playback_and_record
Br
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.