2020-10-12 10:32 AM
I want to be absolutely sure, so should T_NRST be connected to CPU reset. (In this case STM32H750.)
Solved! Go to Solution.
2020-10-12 2:19 PM
The T_* prefix stands for target. It should be connected to the NRST pin of the MCU you're programming.
2020-10-12 2:19 PM
The T_* prefix stands for target. It should be connected to the NRST pin of the MCU you're programming.
2020-10-12 8:34 PM
I see. The plain old reset pin. Some application notes mention also other reset signal which goes to PB4 pin. Jtag reset probably.
2024-08-07 1:33 PM
I normally have NRST on MCU connected to 3.3V directly. Do I need to include a pull-down resistor if also connecting T_NRST to NRST?
For example,
3.3V — [ 10k ] —- NRST/T_NRST
Excuse the ASCII circuit, I’m on my phone.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.