2020-11-18 7:35 PM
2020-11-18 7:39 PM
Have an St-Link-V3 programmer connected via SWD... and I'm using an unused sector for saving data collected.
However, neither Stm32 CUbe Programmer nor St-Link Utility seems to let me dump more than just the active window worth of data.
Is there any St or 3rd party tool that I can read sector(s) worth of data to a file? I don't have any security option set when originally flashed.
Ideally, I would like to put the board in bootloader mode, and read the flash via SERIAL rather than SWD, but at this point , I can use whatever works!
2020-11-19 3:38 AM
Start any programm (e.g. stlink gdb server, openocd, pyocd, bl*ckm*g*ic and more) that starts a gdb server, connect to gdb and dump the binary. Most of this programm also have a mode to read content direct, e.g with bl*ckm*g*x hosted "bl*ckm*g*c -S 0x80000 <file>" will read 512 kB starting at 0x08000000.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.