Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I've made a mistake and programmed to STM32h745 dual core processor program which was created to STM32H743 with one core. Now I have a problem with connection and ST-Link doesn't recognize device. What can I do with that?I've also tried to supply boa...
Only schematic of STM32H743ZI is available, not for STM2H743ZI2, how can I get schematic diagram of STM2H743ZI2 ?
Hi!I burned Stlink-V3 ic(u1-MB1440) while debugging.Maybe I entered the wrong power source.Can you tell me? What's the part number? I couldn't find a part list or a circuit diagram of the mb1440 board.
Hi,I just wanted to debug my STM32L412 custom board using my Nucleo-F767 as ST-Link just as I did many times before.But this time it won't work! Connecting to the board always yields an Error in initializing ST-LINK device. Reason: No device found on...
Hello everybody,I made for school a custom stm32f103C8Txxx board. Programming with a ST-Link V2 work without a problem.To test the pcb, there are 2 led's (pin pc13 en pa10), they both illuminate every 500ms (easy code to test functionality).The code ...
Hi, I'm new in the STM32 world. I recently bougth the STM32L031K6 nucleo board and I am doing a project where I need to connect the analog reference to a voltage different from VDD. So I de-soldered the solder bridge that connects AREF to VDD (SB10)....
Hi,I stumbled on the ST-LINK server in the ST website (https://www.st.com/en/development-tools/st-link-server.html).I was hoping it's their cross-platform GDB-server, supporting Windows/Linux.The popular st-util (by stlink) doesn't satisfy my needs.S...
Was able to program the board previously, but today after updating my STM32CubeIDE, it refused to run debug until I updated the stlink on my dev board.But upon doing so, it gave these error. Essentially meaning I cannot program my dev board.```STMicr...
Is it ok to connect boot0 from STM32 (with a 10k pulldown to GND) to one of pin 1 or 2 on STDC14 from STLINK-V3SET?The pins are 'reserved' regarding to the STLINK-V3SET manual p. 23 with the comment 'Do not connect on target' ;)The boot0 should be ig...
i am using windows 7 os and i have installed stm32cube(1.4) ide and i tried to flash the software to the discovery board but it is not flashed since it has been showing "ST link not detected!please connect ST-Link and restart the program".even i didn...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.