2026-05-01 10:38 AM - last edited on 2026-05-11 12:19 AM by KDJEM.1
I purchased a STM32H745I-DISCO. The board appears to work fine. I am trying to flash the stock firmware onto the board. I downloaded the binary from the ST product page, followed the instructions, set the correct option bytes, used the external loader. The binary file on the product page "STM32Cube_Demo-STM32H745I-DISCO-V1.0.0_FULL.hex" does not bring the board back to factory settings. The touchscreen does not work. The stock demo wont run. Does anyone have have a more up to date binary file or procedure for factory reset?
Thanks
Solved! Go to Solution.
2026-05-04 8:02 AM
Hello,
please download the attached file.
You have to flash it with the STM32Cubeprogrammer using the MT25TL01G_STM32H745I-DISCO external loader.
You can use the GUI to flash the hex file after ensuring you've selected the right external loader:
or execute the command line while you're in the STM32CubeProgrammer\bin folder :
STM32_Programmer_CLI.exe -c port=SWD mode=UR -el ExternalLoader\MT25TL01G_STM32H745I-DISCO.stldr -d Your_path\STM32Cube_Demo-STM32H745I-DISCO-V1.1.0_FULL_V4.hex -v -hardrst
Please let me know whether it helps.
2026-05-04 8:02 AM
Hello,
please download the attached file.
You have to flash it with the STM32Cubeprogrammer using the MT25TL01G_STM32H745I-DISCO external loader.
You can use the GUI to flash the hex file after ensuring you've selected the right external loader:
or execute the command line while you're in the STM32CubeProgrammer\bin folder :
STM32_Programmer_CLI.exe -c port=SWD mode=UR -el ExternalLoader\MT25TL01G_STM32H745I-DISCO.stldr -d Your_path\STM32Cube_Demo-STM32H745I-DISCO-V1.1.0_FULL_V4.hex -v -hardrst
Please let me know whether it helps.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.