2026-04-30 11:08 PM
Hi,
I am using NUCLEO-U545RE-Q with X-NUCLEO-NFC07A1.
After downloading a program via Arduino IDE, the board got locked.
Symptoms:
What I tried:
Questions:
This board is for a competition. Any help is appreciated. Thanks.
2026-05-04 6:34 AM
Hello,
>> How can I unlock or erase this board without a BOOT0 jumper? It seems not available on this NUCLEO board.
BOOT0
BOOT0 can be set to 1 on CN7 connector by bridging pin 5 and pin 7.
BOOT0 is also dependant of the option bytes nBOOT0 and nSWBOOT0:
>> PC cannot detect the board, no ST-LINK device, no COM port
LD3 is off meaning the ST-Link has not activated the T-PWR_EN signal.
Please, check the quality of the USB cable, and if it is not a charger only cable with no D+/D- data lines.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.