2025-04-28 5:19 AM
Is there any information for the STM32H735-DK on how to configure the S70KL128 HyperRAM to work?
Unfortunately, there's no source code for the binary demo from ST, so I'm forced to try to get the HyperRAM working somehow.
And the forums only provide information about problems when trying to run it in memory-mapped mode.
So far, I haven't been able to read or write a single byte because:
- The access times, latency times, and the clock in the STM32H7 must be set correctly for the HyperRAM to be accessible at all.
- The settings in the HyperRAM itself also need to be configured (DDR/DTR, drive strength, latency, burst length).
When creating a new project with the default values in the STM32CubeIDE for the evaluation board, adjust the octospi clock to 100MHz (PLL2R) and attempting to read the hyperram with the debugger, the only output is:
Could not halt device (18)
Failed to read all registers from target
Target is not responding, retrying...
Target is not responding, retrying...
When importing parts from the STM32H7B3I evaluation board and setting the timing, I can actually read incorrect data without the debugger crashing.
Does anyone know what needs to be set for the generic parameters for the octospi2?
Generic
Fifo Threshold 1? or 4?
Device Size 32? 24? 128?
Chip Select High Time 1? 4?
Free Running Clock Disable? Enabled?
Clock Prescaler 1 (at 100MHz Clock ok)
Sample Shifting None ? Half Cycle?
Delay Hold Quarter Cycle Disable ? Enabled?
Chip Select Boundary 31 ? 0? 1? 20?
Delay Block Disable? Enabled?
Maximum Transfer 0 ? 64? 128000?
Refresh Rate 200 ? 64? 32?
HyperBus(TM)
RW Recovery Time 7? or 4? or 6?
Access Time 4? or 0?
Write Access Latency Enable ? Disable ?
Latency Mode Variable ? Fixed?
Has anyone a sourcecode snippet, to initialice the octospi2 (with working parameters like above) and to initialice the S70KL128 to get the hyperram working?
Solved! Go to Solution.
2025-04-28 8:22 AM - edited 2025-04-28 8:23 AM
Hello @Heinz_Baumer;
The STM32H735-DK HyperRAM example is available on STM32CubeH7.
So, I recommend you to look at OSPI_HyperRAM_MemoryMapped example and check the memory configuration.
This example describes how to write and read data in memory-mapped mode in the OCTOSPI HyperRAM memory and compare the result with an intensive access.
The HyperRAM memory used in this example is an S70KL1281 memory.
Also, I advise you before starting with OCTOSPI interface to check the STM32H735 errata sheet and precisely section 2.8 OCTOSPI
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-28 8:22 AM - edited 2025-04-28 8:23 AM
Hello @Heinz_Baumer;
The STM32H735-DK HyperRAM example is available on STM32CubeH7.
So, I recommend you to look at OSPI_HyperRAM_MemoryMapped example and check the memory configuration.
This example describes how to write and read data in memory-mapped mode in the OCTOSPI HyperRAM memory and compare the result with an intensive access.
The HyperRAM memory used in this example is an S70KL1281 memory.
Also, I advise you before starting with OCTOSPI interface to check the STM32H735 errata sheet and precisely section 2.8 OCTOSPI
I hope this help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.