2026-02-13 7:26 AM - last edited on 2026-02-13 9:31 AM by mƎALLEm
Heyho,
just found that the N6 has gigabit ethernet - which might help me staying away from the monstrous MPUs... :D
Is there kinda compatibility list between the STM32 families for the peripherals?
Merci!
Solved! Go to Solution.
2026-02-13 9:40 AM - edited 2026-02-14 3:55 AM
Hello,
Not obvious to provide an exhaustive list of peripherals compatibility between N6 and H7.
Generally speaking, new products feature either the same previous versions of the peripherals from older products, or newer versions with new features or completely new architecture features which is the case of the Eth.
For ADC, Timers, UARTs most probably they are the same, may be with a slight difference in term of triggers and connections with other DMAs.
I think better, to speed up your findings, is to look at the first chapter "main features" in the RMs of each peripheral description and compare + do a comparison of register mapping at the end of the chapter.
2026-02-13 8:06 AM - edited 2026-02-13 8:07 AM
More generally, it would be useful to have this across all families for all the IP blocks.
I think @waclawek.jan has brought this up before ...
PS:
Might be a good question to ask the new ST Sidekick AI agent ...
2026-02-13 9:40 AM - edited 2026-02-14 3:55 AM
Hello,
Not obvious to provide an exhaustive list of peripherals compatibility between N6 and H7.
Generally speaking, new products feature either the same previous versions of the peripherals from older products, or newer versions with new features or completely new architecture features which is the case of the Eth.
For ADC, Timers, UARTs most probably they are the same, may be with a slight difference in term of triggers and connections with other DMAs.
I think better, to speed up your findings, is to look at the first chapter "main features" in the RMs of each peripheral description and compare + do a comparison of register mapping at the end of the chapter.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.