2025-12-12 11:27 AM
Hi, just bought a STLINK-V3SET to use with EVSPIN32G02Q1S1 evaluation board.
It doesn't seem to be able to connect via USB. I've previously recently used STLINK v2ISOL and it worked as expected, so i already had the driver installed and it should be the same driver.
Tried different cables, different PCs, different USB ports, reinstalling the driver: to no avail.
So what can be the reason here? I'd appreciate any suggestions.
2025-12-12 11:31 AM
Some additional info:
when i connect the device to the computer, there is no reaction.
No "device connected" sound, no new devices in the device manager.
The LEDs are both on; the red one (COM) is blinking and the green one is continiously one (PWR).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.